cancel
Showing results for 
Search instead for 
Did you mean: 

i2c3 not probe

guansonghuang
Associate III

hi,

   I found stm32mp135faf7 MPU's i2c3 is not be probed

1、"ovti,ov5640" probe() function no enter

2、not found i2c3 in /sys/class/i2c-dev/

here is my dtsi:

&i2c3 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c3_pins_mx>;
pinctrl-1 = <&i2c3_sleep_pins_mx>;
status = "okay";

i2c-scl-rising-time-ns = <170>;
i2c-scl-falling-time-ns = <5>;
clock-frequency = <100000>;
/delete-property/ dmas;
/delete-property/ dma-names;
ov5640: ov5640@3c{
compatible = "ovti,ov5640";
reg = <0x3c>;
clocks = <&clk_ext_camera>;
clock-names = "xclk";
DOVDD-sup = <&vdd>;
//reset-gpios = <&gpioh 4 (GPIO_ACTIVE_LOW | GPIO_PUSH_PULL)>;
rotation = <180>;
status = "okay";

port {
ov5640_0: endpoint {
remote-endpoint = <&dcmipp_0>;
bus-width = <8>;
bus-type = <5>;
data-shift = <2>;
hsync-active = <0>;
vsync-active = <0>;
pclk-sample = <1>;
pclk-max-frequency = <77000000>;
};

}

2 REPLIES 2
PatrickF
ST Employee

Hi @guansonghuang 

maybe have a look at this page which help to debug this kind of issue (example for UART, but should be similar for I2C)

https://wiki.st.com/stm32mpu/wiki/Trace_and_debug_scenario_-_UART_issue

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
guansonghuang
Associate III

Thank you very much.this helpful