2020-01-16 7:18 AM
Following instructions @
https://www.emsyslabs.com/how-to-compile-linux-using-yocto-for-stm32mp1/
and
https://koansoftware.com/yocto-project-meta-layer-for-stm32mp1-by-koan/
I'm led to believe that a qtcreator executable or script will be created which I can run on the host (Debian) to create and cross compile a QT5 app for STM32MP157.
I'm new to QT but need to create a simple UI to run on STM32MP157, what am I missing ?
Thanks in advance.
Solved! Go to Solution.
2020-01-22 5:38 AM
Hi @wpaulilkinson the QtCreator is an independent executable. It is an IDE provided by Qt (see their website).
If you want to build cross-compiling Qt code using QtCreator you have to setup the cross compilation environment before you call QtCreator.
To do that you have two options: 1. open a terminal, setup environment, call Qtcreator; 2. add the cross compilation environment script into a script.
I usually prefer to copy the existing script Qt/Tools/QtCreator/bin/qtcreator.sh and modify it
cp Qt/Tools/QtCreator/bin/qtcreator.sh Qt/Tools/QtCreator/bin/qtcreator-stm32.shand insert a line like that (you have to adapt it to your cross compiler)
#! /bin/bash
# Bourne shell(sh), use the . command to source a file
. /opt/st/stm32mp1-disco/2.6-snapshot/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabiDistinti Saluti / Best Regards
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
Phone: +39 035-255235
2020-01-17 5:14 AM
Hi @wpaulilkinson
Do you mean that you didn't get the script and executable as described in point 17 of https://www.emsyslabs.com/how-to-compile-linux-using-yocto-for-stm32mp1/ ?
Or this results is not your expectation ?
Thanks for clarification.
Olivier
2020-01-17 5:48 AM
Thanks Oliver,
Neither the executable stm32_qtcreator or script stm32_qtcreator.sh are created, well not on my desktop or in /opt/st/stm32mp1/2.6-snapshot.
environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi is present in /opt/st/stm32mp1/2.6-snapshot.
My expectation is that both script and executable should be created.
Best regards,
Paul.
2020-01-22 5:38 AM
Hi @wpaulilkinson the QtCreator is an independent executable. It is an IDE provided by Qt (see their website).
If you want to build cross-compiling Qt code using QtCreator you have to setup the cross compilation environment before you call QtCreator.
To do that you have two options: 1. open a terminal, setup environment, call Qtcreator; 2. add the cross compilation environment script into a script.
I usually prefer to copy the existing script Qt/Tools/QtCreator/bin/qtcreator.sh and modify it
cp Qt/Tools/QtCreator/bin/qtcreator.sh Qt/Tools/QtCreator/bin/qtcreator-stm32.shand insert a line like that (you have to adapt it to your cross compiler)
#! /bin/bash
# Bourne shell(sh), use the . command to source a file
. /opt/st/stm32mp1-disco/2.6-snapshot/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabiDistinti Saluti / Best Regards
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
Phone: +39 035-255235
2020-01-23 5:48 AM
Thanks Marco,
Your answers make sense and tie up with the results of 'bitbake meta-toolchain-qt5 ' in my environment.
In the interim I used Qtcreator to create a simple QT5 UI and created a recipe to cross compile the code.
Best regards,
Paul.
2020-05-07 10:30 AM
Hi Marco and Paul,
I have installed qtcreator and sourced the correct script from step 17 before calling qtcreator. But After setting up my device kit in qt I get errors as if qt is still trying to compile for my x86 64 bit Linux host. Is there a special way I have to install qtcreator?
main.o: file not recognized: file format not recognized
Thanks for the help