2025-01-12 7:51 AM
Hi , I built openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27 (openstlinux-eglfs), SDK, configure QtCreator and prepare my first app, but some library mising on target device - STM32MP157F-DK2. Below log, after deploy:
id: 'weston': no such user
id: 'weston': no such user
QML debugging is enabled. Only use this in a safe environment.
QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/tmp/runtime-root'
No modes available for output "HDMI1"
qt.qpa.input: xkbcommon not available, not performing key mapping
QQmlApplicationEngine failed to load component
qrc:/qml/dashboard.qml:55:1: module "QtQuick.Extras" is not installed
qrc:/qml/dashboard.qml:54:1: module "QtQuick.Controls.Styles" is not installed
qrc:/qml/dashboard.qml:53:1: module "QtQuick.Controls" is not installed
qrc:/qml/dashboard.qml:55:1: module "QtQuick.Extras" is not installed
qrc:/qml/dashboard.qml:54:1: module "QtQuick.Controls.Styles" is not installed
qrc:/qml/dashboard.qml:53:1: module "QtQuick.Controls" is not installed
qrc:/qml/dashboard.qml:55:1: module "QtQuick.Extras" is not installed
qrc:/qml/dashboard.qml:54:1: module "QtQuick.Controls.Styles" is not installed
qrc:/qml/dashboard.qml:53:1: module "QtQuick.Controls" is not installed
11:20:13: Remote process crashed.
How install missing library on target device ?
Solved! Go to Solution.
2025-01-16 10:33 AM
Problem solved , by adding in local.conf:
IMAGE_INSTALL:append = "qtquickcontrols qtquickcontrols-qmlplugins qtquickcontrols2 qtquickcontrols2-qmlplugins"
and run bitbake
2025-01-16 10:33 AM
Problem solved , by adding in local.conf:
IMAGE_INSTALL:append = "qtquickcontrols qtquickcontrols-qmlplugins qtquickcontrols2 qtquickcontrols2-qmlplugins"
and run bitbake
2025-01-18 1:04 AM
How can I install next missing library ? --> libQt5SerialBus.so.5 ?
2025-01-18 3:47 AM
Problem solved by adding:
IMAGE_INSTALL:append = " qtserialbus qtserialport"