How to setup FDCAN on STM32MP157F-DK2?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-11-22 9:59 AM
Hi everyone!
I'm here with my devkit and trying to have FDCAN working properly! I compiled the Yocto distribution for the board and I followed all the tutorials in the wiki ( https://wiki.st.com/stm32mpu/wiki/Category:CAN ) and here's what I came up with:
I initialized m_can1
&m_can1 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&m_can1_pins_b>;
pinctrl-1 = <&m_can1_sleep_pins_b>;
status = "okay";
};
I used the pins_b configuration because looking at the datasheet they were the only possible exposed pins on the PI_GPIO extender (CN2) on the board (overwriting I2C5 pins for the Arduino). I also removed the pullup resistors for i2c (R166 and R167).
On the kernel side I tried the loopback and seems to work fine:
root@stm32mp1:~# ip link set can0 up type can bitrate 1000000 dbitrate 2000000 fd on
[ 1602.982564] m_can_platform 4400e000.can can0: bitrate error 0.3%
[ 1602.988958] m_can_platform 4400e000.can can0: bitrate error 0.3%
[ 1602.994593] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready
(the second bitrate error is different from the tutorials...) and seems working ok
root@stm32mp1:~# candump can0 -L &
root@stm32mp1:~# cansend can0 300#AC.AB.AD.AE.75.49.AD.D1
(1669130989.509567) can0 300#ACABADAE7549ADD1
(1669130989.509533) can0 300#ACABADAE7549ADD1
Now, I'm trying to get some data on the physical bus but it seems not working, I attached the oscilloscope on the pin PA12 (EXP_GPIO2) which should be the FDCAN tx, and enabled the bus as the example :
ip link set can0 up type can bitrate 1000000 dbitrate 2000000 fd on
But I can see absolutely nothing on the pin if I send any packet with cansend.
I also tried to attach a proper transceiver ( I used mikro CAN FD 3 click https://www.mikroe.com/can-fd-3-click --> TLE9251V based) , and after the cansend, the bus goes instantly bus-off :
root@stm32mp1:~# cansend can0 01a#11223344AABBCCFF
[ 706.810510] m_can_platform 4400e000.can can0: bus-off
Do you have any suggestions to make the protocol work properly? Do you have tried it yourself?
Huge thanks!
Simone
Solved! Go to Solution.
- Labels:
-
CAN
-
FDCAN
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-11-23 3:03 AM
For transceiver MCP2542 following pins have to be connected:
* 3.3V
* 5V
* GND
* TX to MC2542 RX
* RX to MC2542 TX
Note: Do not forget to cross TX/RX!
Function STM32 pin Pin To MCP
3V3 - 1 3V3
5V - 2 5V
GPIO2 PA12 3 RX
GPIO3 PA11 4 TX
GND - 9 GND
This worked for me.
Bye Gunther
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-11-23 3:03 AM
For transceiver MCP2542 following pins have to be connected:
* 3.3V
* 5V
* GND
* TX to MC2542 RX
* RX to MC2542 TX
Note: Do not forget to cross TX/RX!
Function STM32 pin Pin To MCP
3V3 - 1 3V3
5V - 2 5V
GPIO2 PA12 3 RX
GPIO3 PA11 4 TX
GND - 9 GND
This worked for me.
Bye Gunther
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-11-23 3:16 AM
Hi @GLaure​
thanks for the answer! I din't attach both alimetations, I'll try that.
I have some questions: did you enable m_can only in the kernel dts just like me, or also in uboot? Also, did you removed the resistors as I did? Did you follow the same steps I did?
Thank you SO MUCH
simone
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-11-23 3:18 AM
Just in the kernel dts. It does not have to be configured by u-boot.
I did not remove any resistors.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-11-23 3:19 AM
Ok thanks... i'll try then
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-11-23 7:20 AM
Hi @GLaure​,
You were right! I reattached the resistors, plug both powers 3v3 and 5v, inverted tx and rx and got the CAN working! I have to fine tuning the sample-points and all others stuff but it works! So we assume that the double alimentation is kinda standard for transcievers. Again, I'm using CAN FD 3 Click an a add-on board based on TLE9251V CAN.
thanks again
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-21 8:46 AM
When working with a CAN transceiver and and MCPU you do not cross TX/RX. It may appear to work, but it will fail as the CAN network grows and there are multiple senders/receivers.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-21 8:53 AM
Yes you're right! Thanks
However, I want to warn who will watch this post saying that with this MPU (also for all MP1 family?) you will loose a lot of time calibrating the clock for FDCAN, by default is imprecise at high baudrates! My suggestion is to initialize the peripheral under the M4 and handling it inside the firmware and not in Linux user space. It's just easier, but it's not mandatory.
See ya
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-21 8:58 AM
I have also found that I can get higher, reliable speeds using the Cortex M7 and M4 cores on the H745 for instance. In this instance I am using 1Mb arbitration and 1Mb data rate and it's working acceptably.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-30 6:14 AM
hi @GLaure
help me out the FDCAN where i saw manual where i unable to find the FDCAN pins how you get the exact location of the pin and i want to receive the data only