2022-06-03 5:14 AM - last edited on 2023-06-16 5:59 AM by Kevin HUBER
Hi!
I am trying to enable PTP on STM32F157 DK2 evaluation board.
From my understanding, pps_available should return 1, (if configured correctly).
root@stm32mp1:~# cat /sys/class/ptp/ptp0/pps_available
0
I added "linuxptp" to the image:
IMAGE_INSTALL_append += " \
linuxptp \
"
I tried to follow the instructions for kernel 4.14:
https://community.st.com/s/question/0D50X0000BMG2RoSQL/how-do-i-enable-linuxptp-pps-output
To enable PPS Out, I also patched stm32mp-mp15-pinctrl.dtsi
diff --git a/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi b/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi
index 236d77e..1e74905 100644
--- a/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi
+++ b/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi
@@ -160,6 +160,7 @@
ethernet0_rgmii_pins_a: rgmii-0 {
pins1 {
pinmux = <STM32_PINMUX('G', 5, AF11)>, /* ETH_RGMII_CLK125 */
+ <STM32_PINMUX('G', 8, AF11)>, /* ETH_PPS_OUT */
<STM32_PINMUX('G', 4, AF11)>, /* ETH_RGMII_GTX_CLK */
<STM32_PINMUX('G', 13, AF11)>, /* ETH_RGMII_TXD0 */
<STM32_PINMUX('G', 14, AF11)>, /* ETH_RGMII_TXD1 */
@@ -191,6 +192,7 @@
ethernet0_rgmii_sleep_pins_a: rgmii-sleep-0 {
pins1 {
pinmux = <STM32_PINMUX('G', 5, ANALOG)>, /* ETH_RGMII_CLK125 */
+ <STM32_PINMUX('G', 8, ANALOG)>, /* ETH_PPS_OUT */
<STM32_PINMUX('G', 4, ANALOG)>, /* ETH_RGMII_GTX_CLK */
<STM32_PINMUX('G', 13, ANALOG)>, /* ETH_RGMII_TXD0 */
<STM32_PINMUX('G', 14, ANALOG)>, /* ETH_RGMII_TXD1 */
--
2.25.1
As far as I could see, the other changes are not longer needed for kernel 5.10.
Still cat /sys/class/ptp/ptp0/pps_available returns 0.
What did I miss?
Any help is greatly appreciated!
Have a nice weekend!
Gunther
Solved! Go to Solution.
2022-08-09 11:11 PM
Good Morning @OlivierK ,
PTP was on hold as I had to get DMA from an FPGA running. This is working now, so will look into PTP again. I will report back :)
Update:
I used this kernel config fragment:
CONFIG_PPS=y
CONFIG_PPS_DEBUG=y
#
# PPS clients support
#
CONFIG_PPS_CLIENT_KTIMER=m
CONFIG_PPS_CLIENT_LDISC=m
CONFIG_PPS_CLIENT_GPIO=mThe CONFIG_PPS_CLIENT_KTIMER has to be configured as a module. If it is buildin (with 'y') pps0 as device is not created.
Then start ptp4l as you described:
ptp4l -l 6 -m -i eth0 -p /dev/ptp0and set the pps duty cycle
echo "0 0 0 1 1" > /sys/class/ptp/ptp0/periodA oszilloscpe now shows the PPS!
Perfect and thank you @OlivierK
Update 2:
Just to be complete:
This is not necessary:
modprobe pps-ktimerBye, Gunther