Hardware: STM32MP1-DK1
Software: Windows STM32Cube Programmer
Question: Download hardware failed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-13 5:57 PM
Hardware: STM32MP1-DK1
Software: Windows STM32Cube Programmer
Question: Download hardware failed.
NOTICE: CPU: STM32MP157AAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
NOTICE: Board: MB1272 Var1.0 Rev.C-01
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: PMIC version = 0x10
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):v2.4-dirty
NOTICE: BL2: Built : 16:43:51, Nov 17 2020
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
ERROR: DDR addr bus test: can't access memory @ 0xc0000004
PANIC at PC : 0x2ffed949
Exception mode=0x00000016 at: 0x2ffed949
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-14 9:41 AM
Hello @�?� 放 ,
I can see that you are using ecosystem v3.0.0. Could you please tell me your version of CubeProgrammer?
And if you have a version lower than 2.7.0, please can you try with a STM32CubeProgrammer 2.7.0 or bigger.
The version that was delivered with the v3.0.0 package is the 2.7.0:
Did you already succeeded to program this board before?
Regards,
Kevin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-14 9:36 PM
v2.9.0 was also failed.
yes, i succeeded to program this board before.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-02-24 2:15 AM
Hello @�?� 放 ,
Sorry for the late reply, it looks like an hardware issue.
This error when reading the DDR at 0xC000004 and the fact that it worked before let me think that.
- Are you able to build your board normally or do you also encounter this error of DDR?
- Do you have a second board to test if your setup and binaries works with the new one?
- You can try to populate your SDCard manually by inserting it in a PC directly:
And test if everything is ok without the download operation.
Regards,
Kévin