cancel
Showing results for 
Search instead for 
Did you mean: 

Can't program eMMC using CubeProgramer with signed & encrypted firmware and FIP

ThinhNguyen
Associate III

Hardware setup:
- STM32MP257F-DK

- The OTP in the chip is burned with the correct OTP value and it is closed.

- Connect CN15 USB Port to a Ubuntu Laptop.

- BOOT0 = BOOT1 = BOOT2 = BOOT3 = 0

- Power on the DEV KIT.

Software:

Enable Secure Boot + Encrypted

ROOT_SIGN_KEY = "/mnt/HDD_2TB/KeyGenSecBoot/stm32mp25-signaturekey" ROOT_ENCRYPT_KEY = "/mnt/HDD_2TB/KeyGenSecBoot/stm32mp25-encryptionkey" # Generate Distribution Package with signed binaries for STM32MP25 SIGN_KEY = "${ROOT_SIGN_KEY}/privateKey00.pem" SIGN_KEY_stm32mp21 = "${ROOT_SIGN_KEY}/privateKey00.pem" SIGN_KEY_stm32mp23 = "${ROOT_SIGN_KEY}/privateKey00.pem" SIGN_KEY_stm32mp25 = "${ROOT_SIGN_KEY}/privateKey00.pem" EXTERNAL_KEY_CONF = "1" SIGN_KEY_PASS = "xxx xxx xxxx xxxx xxxxxx xxx xxx xxx" SIGN_ENABLE = "1" SIGN_TOOL = "/home/thinhnguyen/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32_SigningTool_CLI" # Generate a Distribution Package with encrypted partition binaries for STM32MP25 ENCRYPT_ENABLE = "1" ENCRYPT_FSBL_KEY = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key.bin" ENCRYPT_FSBL_KEY_stm32mp21 = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key.bin" ENCRYPT_FSBL_KEY_stm32mp23 = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key.bin" ENCRYPT_FSBL_KEY_stm32mp25 = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key.bin" ENCRYPT_FIP_KEY = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key_256bits.bin" ENCRYPT_FIP_KEY_stm32mp21 = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key_256bits.bin" ENCRYPT_FIP_KEY_stm32mp23 = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key_256bits.bin" ENCRYPT_FIP_KEY_stm32mp25 = "${ROOT_ENCRYPT_KEY}/stm32mp_encryption_key_256bits.bin"

Build st-image-weston

Flash Layout

#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp257f-dk-optee-programmer-usb_Encrypted_Signed.stm32 - 0x02 fip-ddr FIP none 0x0 fip/fip-stm32mp257f-dk-ddr-optee-programmer-usb_Encrypted_Signed.bin - 0x03 fip-boot FIP none 0x0 fip/fip-stm32mp257f-dk-optee-programmer-usb_Encrypted_Signed.bin PED 0x10 emmcboot0 RawImage mmc1 boot1 none PED 0x11 emmcboot1 RawImage mmc1 boot2 none PED 0x12 emmcall RawImage mmc1 0x0 none PED 0x15 sdcardall RawImage mmc0 0x0 none

Program the DEV KIT via USB Using STM32CubeIDE
At first, STM32CubeProgrammer can connect to the DK via USB. After that, The DEV KIT keeps disconnected after loading arm-trusted-firmware and fip. Below is the log from STM32CubeProgramer.

09:26:54 : Start Embedded Flashing service 09:26:54 : Opening and parsing file: tf-a-stm32mp257f-dk-optee-programmer-usb_Encrypted_Signed.stm32 09:26:54 : Memory Programming ... 09:26:54 : File : tf-a-stm32mp257f-dk-optee-programmer-usb_Encrypted_Signed.stm32 09:26:54 : Size : 191.53 KB 09:26:54 : Partition ID : 0x01 09:26:54 : Download in Progress: 09:26:55 : File download complete 09:26:55 : Time elapsed during download operation: 00:00:01.515 09:26:55 : RUNNING Program ... 09:26:55 : PartID: :0x01 09:26:56 : Reconnecting the device ... 09:26:56 : USB speed : High Speed (480MBit/s) 09:26:56 : Manuf. ID : STMicroelectronics 09:26:56 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0011, /STM32MP257FAK Rev.Y, 09:26:56 : SN : 004600314236501600363847 09:26:56 : DFU protocol: 1.1 09:26:56 : Board : -- 09:26:56 : Device ID : 0x0505 09:26:56 : Device name : STM32MP257FAK Rev.Y 09:26:56 : Device type : 09:26:56 : Device CPU : 09:26:56 : Start operation done successfully at partition 0x01 09:26:56 : Opening and parsing file: fip-stm32mp257f-dk-ddr-optee-programmer-usb_Encrypted_Signed.bin 09:26:56 : Memory Programming ... 09:26:56 : File : fip-stm32mp257f-dk-ddr-optee-programmer-usb_Encrypted_Signed.bin 09:26:56 : Size : 34.34 KB 09:26:56 : Partition ID : 0x02 09:26:56 : Download in Progress: 09:26:56 : File download complete 09:26:56 : Time elapsed during download operation: 00:00:00.070 09:26:56 : RUNNING Program ... 09:26:56 : PartID: :0x02 09:26:57 : Reconnecting the device ... 09:26:57 : USB speed : High Speed (480MBit/s) 09:26:57 : Manuf. ID : STMicroelectronics 09:26:57 : Product ID : DFU @Device ID /0x505, @Revision ID /0x0011, /STM32MP257FAK Rev.Y, 09:26:57 : SN : 004600314236501600363847 09:26:57 : DFU protocol: 1.1 09:26:57 : Board : -- 09:26:57 : Device ID : 0x0505 09:26:57 : Device name : STM32MP257FAK Rev.Y 09:26:57 : Device type : 09:26:57 : Device CPU : 09:26:57 : Start operation done successfully at partition 0x02 09:26:57 : Opening and parsing file: fip-stm32mp257f-dk-optee-programmer-usb_Encrypted_Signed.bin 09:26:57 : Memory Programming ... 09:26:57 : File : fip-stm32mp257f-dk-optee-programmer-usb_Encrypted_Signed.bin 09:26:57 : Size : 2.99 MB 09:26:57 : Partition ID : 0x03 09:26:57 : Download in Progress: 09:27:03 : File download complete 09:27:03 : Time elapsed during download operation: 00:00:06.132 09:27:03 : RUNNING Program ... 09:27:03 : PartID: :0x03 09:27:04 : Reconnecting the device ... 09:27:07 : USB speed : High Speed (480MBit/s) 09:27:07 : Manuf. ID : STMicroelectronics 09:27:07 : Product ID : USB download gadget@Device ID /0x505, @Revision ID /0x0011, /STM32MP257FAK Rev.Y, 09:27:07 : SN : 004600314236501600363847 09:27:07 : DFU protocol: 1.1 09:27:07 : Board : -- 09:27:07 : Device ID : 0x0505 09:27:07 : Device name : STM32MP257FAK Rev.Y 09:27:07 : Device type : 09:27:07 : Device CPU : 09:27:07 : Start operation done successfully at partition 0x03 09:27:07 : Flashlayout Programming ... 09:27:07 : Running Flashlayout Partition ... 09:27:08 : Reconnecting the device ... 09:27:38 : Error: Unable to reconnect the target device: time out expired 09:27:38 : Error: Start Operation failed at Flashlayout partition 09:27:38 : Error: TSV flashing service failed 09:27:38 : Disconnected from device.
View more

 

From the log, I found that the arm-trusted-firmware and fip are downloaded. Afterthat, The board die. I am sure that my OTP and device closing are correct because the board can boot from SD card with Signed and Encryted boot loader. Please help with this issue.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
ThinhNguyen
Associate III

I seems the process is done successfully. It may not delete all eMMC, just nesesary sectors.

09:27:07 : Start operation done successfully at partition 0x03 09:27:07 : Flashlayout Programming ... 09:27:07 : Running Flashlayout Partition ...

View solution in original post

1 REPLY 1
ThinhNguyen
Associate III

I seems the process is done successfully. It may not delete all eMMC, just nesesary sectors.

09:27:07 : Start operation done successfully at partition 0x03 09:27:07 : Flashlayout Programming ... 09:27:07 : Running Flashlayout Partition ...