2020-11-12 2:39 PM
Hello,
I tried to apply the step by step "Modify, rebuild and reload the Linux® kernel" form wiki.st .
Everything works fine from the first step of the "Getting started " until i uncoutered the error bellow.
Unfortunately i am a complete beginner on these tools and don't understand whats happen.
Thank you by advance for any help.
@PC:~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.31-r0/linux-5.4.31$ make ARCH=arm multi_v7_defconfig "fragment*.config"
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
HOSTCC scripts/kconfig/confdata.o
HOSTCC scripts/kconfig/expr.o
LEX scripts/kconfig/lexer.lex.c
/bin/sh: 1: flex: not found
scripts/Makefile.host:9: recipe for target 'scripts/kconfig/lexer.lex.c' failed
make[2]: *** [scripts/kconfig/lexer.lex.c] Error 127
Makefile:567: recipe for target 'multi_v7_defconfig' failed
make[1]: *** [multi_v7_defconfig] Error 2
Makefile:326: recipe for target '__build_one_by_one' failed
make: *** [__build_one_by_one] Error 2
Solved! Go to Solution.
2021-01-21 11:41 AM
Thanks @Sisyphus38 , when I repeated the reinstallation, I kept a close eye on the messages fired back and I realized some of the modules were not being installed because of storage space. So I increased the virtual disk in my VMWare from 20GB to 50GB and everything went on smoothly to the end, the only problem still troubling me is that the board returns an IPv6 address only, while the instructions show as if I have to use IPv4.
So now I get stuck on this command trying to communicate between my laptop and the board
2021-01-22 1:09 AM
Hello MSele.1,
Good news !
I have noticied the same situation. That moment I thaugth the device is only IPv6 Compatible, but i was wrong.
If I am right your host developpement computer needs to attribute an ipv4 adress. So you have to adjust network parameters in the host computer like DHCP, subnetwork mask....
Maybe this link can help you.
https://www.cyberciti.biz/faq/linux-unix-ifconfig-does-not-show-ip-address/
Don't hesitate to give feedback for other users.
Regards
2021-01-22 3:20 AM
Sorry MSele1, post sent twice.
2021-01-22 5:03 AM
Hi @Sisyphus38 ,
I deleted the duplicate comment.
@MSele.1 ,
To get ipv4 address seems you have to set :
[Network]
DHCP=ipv4in some conf file in /lib/systemd/network
See https://wiki.st.com/stm32mpu/wiki/How_to_configure_ethernet_interface
Hope it help,
Olivier
2021-01-25 4:19 AM
Hi @Community member I was unable to connect my pc to the board using ethernet, because of IP differences. Resolving between IPv4 and IPv6 has become too complicated for me since the board has no editor that I can use to edit the files indicated at the link you provided; in future I will use a router between my pc and the board, but I need this problem to be solved now before I get the router. My work around was by copying to a USB memory stick all files that were supposed to be sent by the command
PC $> scp arch/arm/boot/dts/stm32mp157*.dtb root@<board ip address>:/boot
in Section 5.2 here Modify, rebuild and reload the Linux® kernel - stm32mpu and transfer them to the board manually.
The problem comes again as a I move to Section 5.3 where the command
PC $> find install_artifact/ -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
fires the following error
If I ignore that error and proceed by copying all files intended by the command
PC $> scp -r install_artifact/lib/modules/* root@<ip of board>:/lib/modules
then I run into memory problems where many modules of the kernel cannot be installed because of insufficient space as shown below.
Do you have any ideas to go around it? Please @Community member and @Sisyphus38 help with your expertise and experience with this board
2021-01-25 5:38 AM
Hi @MSele.1 ,
Did you remove busybox/"vi" editor support from the target ?
Olivier
2021-01-25 5:43 AM
@Community member No, and I don't know what is that! I was trying to use gedit
2021-01-25 6:00 AM
"vi" is a very basic but famous light text editor.
It present by default in OpenSTLinux.
Make a try and consult the web for a "vi cheat sheet" in order to get command syntax.
basically
vi file
move to the line to edit with arrow
hit key "i" to insert
type the text
escapte + :wq ( for write + quit) and that's done
-> in case of any error :q! to quit without saving
Olivier
2021-01-25 6:04 AM
@Community member
I got that "vi" one and I already have read its basic commands; I will go back to the setup later. However, at this moment I want to resolve the following problem to reduce the required memory space
PC $> find install_artifact/ -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
2021-01-26 8:25 AM
@Community member and @Sisyphus38
Thank you for your help. I got through all my problems now. All I did was to connect the Laptop to the board through a switch (router) and everything went smoothly. Initially I was connecting the laptop directly to the board, and it seems this laptop cannot implement DHCP services.
However, I've got another serious problem that following the instructions of Section 6 to recompile the kernel as presented at Modify, rebuild and reload the Linux® kernel - stm32mpu
Now the board is failing to load the recompiled kernel; it stops here and restarts again.
Any advise how to address it?