cancel
Showing results for 
Search instead for 
Did you mean: 

Enable i2c7 STM32MP25

saarpartush
Associate II

Hi,

I am working on custom board with STM32MP257. I am trying to enable i2c7 but it is RIFSC blocked.

When I try to change the rif configuration for i2c7 the flashing process is interrupted and I cannot download the FW.

Any help would be appreciated.

Thanks.

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @saarpartush 

Can you please share console trace when flash process interrupted ? 

Thanks

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Sure. Here it is:
FO: PMIC2 version = 0x11
INFO: PMIC2 product ID = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0xe011000
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.10-stm32mp2-r1.0(debug):lts-v2.10.5-dirty(7c229848)
NOTICE: BL2: Built : 16:19:31, Jun 28 2024
INFO: EventBuffer0: BuffArea=e03f000 DmaAddr=0e03f000 CoherentMapAddr=0xe03f000
INFO: dwc3_set_dev_speed = HighSpeed
INFO: DFU USB START...
INFO: Event: Link Status Change : ON(0)
INFO: Event: Link Status Change : Early Suspend(5)
INFO: Event: Link Status Change : L2(3)
INFO: Event: Suspend
INFO: USB Suspend mode
INFO: Event: Device Reset
INFO: Event: Device Connection Done
INFO: dwc3_get_dev_speed = HighSpeed
INFO: Event: Link Status Change : ON(0)
INFO: phase ID :2, Manifestation 0 at e007584
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0xe041000
INFO: Image id=26 loaded: 0xe041000 - 0xe048524
INFO: BL2: Doing platform setup
INFO: RAM: DDR4 2x16Gbits 2x16bits 1200MHz
INFO: Memory size = 0x100000000 (4096 MB)
INFO: DFU USB START...
INFO: Event: Link Status Change : ON(0)
INFO: Event: Link Status Change : Early Suspend(5)
INFO: Event: Link Status Change : L2(3)
INFO: Event: Suspend
INFO: USB Suspend mode
INFO: Event: Device Reset
INFO: Event: Device Connection Done
INFO: dwc3_get_dev_speed = HighSpeed
INFO: Event: Link Status Change : ON(0)
INFO: phase ID :3, Manifestation 1 at 872fcfd7
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0xe000000
INFO: Image id=1 loaded: 0xe000000 - 0xe000326
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0xe000000
INFO: FCONF: Reading firmware configuration information for: risaf_config
INFO: RISAF2: No configuration in DT, use default
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: BL31 max size = 0x17000 (94208B)
INFO: BL2: Loading image id 3
INFO: Loading image id=3 at address 0xe000000
INFO: Image id=3 loaded: 0xe000000 - 0xe0135b0
INFO: BL2: Loading image id 19
INFO: Loading image id=19 at address 0x81fc0000
INFO: Image id=19 loaded: 0x81fc0000 - 0x81fc39b9
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x82000000
INFO: Image id=4 loaded: 0x82000000 - 0x8200001c
INFO: OPTEE ep=0x82000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x1
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0x82000000
INFO: Image id=8 loaded: 0x82000000 - 0x820fd628
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0x84400000
INFO: Image id=2 loaded: 0x84400000 - 0x8441c688
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0x84000000
INFO: Image id=5 loaded: 0x84000000 - 0x841c49b8
NOTICE: BL2: Booting BL31
INFO: Entry point address = 0xe000000
INFO: SPSR = 0x3cd
INFO: ARM GICv2 driver initialized
NOTICE: BL31: v2.10-stm32mp2-r1.0(debug):lts-v2.10.5-dirty(7c229848)
NOTICE: BL31: Built : 16:19:31, Jun 28 2024
INFO: BL31: Initializing runtime services
INFO: BL31: Initializing BL32