cancel
Showing results for 
Search instead for 
Did you mean: 

Connect a debugger to STM32MP257F-EV1 board

Aiyps
Associate II

Hi,

At my company, we develop debuggers and are trying to access STM32MP257F-EV1(ES) board via the DAP,
Unfortunately, we are unable to access the DAP and it seems like JTAG (DAP) access is prohibited by hardware
.
The result was the same even after shorting JP3 and turning off ST-LINK.

I have the following questions:

  1. Are there any other jumpers positions that have to be changed? Please let me know.
  2. Does STM32MP257F-EV1(ES) have debug authentication enabled by default?
    If so, please let me know if there are any technical documents that explain the procedure for debug authentication.
  3. I tried to connect to the on-board debugger by running STM32CubeProgrammer and choosing ST-LINK (SWD), but access was denied.
    The boot mode that I tried were "UART/USB" and "Development", but both showed the following error:
    Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
    Please let me know if there is a document or URL that explains how
    STM32CubeProgrammer can be used to access STM32MP257F.

I would appreciate any response.
Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

in 'development boot' (BOOT=0b0011 or 0b1100), the debug is enabled and nothing specific is needed to access thru JTAG/SWD. In development boot, the red led (LD1, close to reset button) is light.

As you are building debuggers for ST chipset, There is maybe some partnership already in place. Could you give me more details on your company and if you get the board through distributor or directly from ST (by private message if you prefer).

If it helps, here is part of the T32 initialisation I use:

SYStem.RESetOut

wait 100.ms

; Cortex-A35
sys.cpu CortexA35

; JTAG/SWD freq
system.JTAGCLOCK 2M
SYSTEM.CONFIG.DEBUGPORTTYPE SWD
SYStem.CONFIG SWDP ON

; DAP Config
sys.config CHIPIRPRE 4.
sys.config CHIPDRPRE 1.
sys.config DAPIRPOST 5.
sys.config DAPDRPOST 1.

; Dual core (A35)
system.CONFIG.CoreNumber 2.

;Assign the two CA35 to this debug session
core.assign 1. 2.

; Debug base address for each core
SYStem.CONFIG.COREDEBUG.Base DAP:0x80210000 DAP:0x80310000

; Config access ports
SYStem.CONFIG MEMORYACCESSPORT 0.
SYStem.CONFIG AHBACCESSPORT 0.
SYStem.CONFIG APBACCESSPORT 0.
SYStem.CONFIG DEBUGACCESSPORT 0.
SYStem.CONFIG AXIACCESSPORT 4.

sys.o.WaitReset 1.s

sys.o.EnReset OFF
sys.o.ResBreak OFF

; connect DAP only
SYStem.Mode.Prepare

; Disable vector catch
tronchip.reset
tronchip.set reset off
tronchip.set StepVector off

; Attach and halt
sys.mode.up
if run()
	break.

 

I you cannot progress, maybe ask for direct support to your local ST representative.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

7 REPLIES 7
PatrickF
ST Employee

Hi @Aiyps 

please see some answers:

1. JP3 is not needed to allows 3rd party debugger access thru CN22. You could keep JP3 off to use STLINK VCP for console(s) even with CN22 usage

2. There is no debug authentication, but debug is not enabled in all cases. 'Development boot' could be used to debug (or need to have a SW running which enable the debug inside BSEC)

3. Unlike STM32MCUs, CubeProgrammer cannot be used with STLINK. Only USB or UART is available for download binaries. STLINK is only for debugging purpose (e.g. CubeIDE) and to show UART VCP for serial console(s)

CubeProgrammer should work to download Starter Package into flash (with adequate BOOT pins). See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image

 

I personally use a 3rd party debugger (Lauterbach Trace32 PowerDebug) on EV board without issues.

 

Could you please precise which board revision (MB1936x) and which device revision (B, X or Y, seen on top of  STM32MP257 package) you have ?

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Hi @PatrickF  

Thank you for your reply.
Please find the details of the board below:

  • Main Board: MB1936-MP257F_X-C01
  • Chip details: "ES2MP257F AI3 - AA042 9R B - TWN 3R 410 - 05". "E2" is mentioned on the top.
    I have attached the photo of the package for your reference.
    Aiyps_1-1723007143942.png

Note that the STM32MP257F-EV1 board has a sticker with "ES" on it. 

 

Thank you, I understand that CubeProgrammer cannot be used via ST-LINK to debug and can only be used to flash images. We will try to use STM32CubeIDE instead via ST-LINK(SWD).

Since you are able to perform debug by connecting Lauterbach Trace32 PowerDebug via the MIPI10 connector (CN22) of the STM32MP257F-EV1, could you please let me know if there is any procedure to be followed (jumper, boot mode etc.) when
Lauterbach debugger is used.

We thought that when the board is booted using 'Development boot', JTAG (DAP) would be enabled. But unfortunately access is denied.

I would appreciate any help with regard to this.

Thank you again.

Hi,

in 'development boot' (BOOT=0b0011 or 0b1100), the debug is enabled and nothing specific is needed to access thru JTAG/SWD. In development boot, the red led (LD1, close to reset button) is light.

As you are building debuggers for ST chipset, There is maybe some partnership already in place. Could you give me more details on your company and if you get the board through distributor or directly from ST (by private message if you prefer).

If it helps, here is part of the T32 initialisation I use:

SYStem.RESetOut

wait 100.ms

; Cortex-A35
sys.cpu CortexA35

; JTAG/SWD freq
system.JTAGCLOCK 2M
SYSTEM.CONFIG.DEBUGPORTTYPE SWD
SYStem.CONFIG SWDP ON

; DAP Config
sys.config CHIPIRPRE 4.
sys.config CHIPDRPRE 1.
sys.config DAPIRPOST 5.
sys.config DAPDRPOST 1.

; Dual core (A35)
system.CONFIG.CoreNumber 2.

;Assign the two CA35 to this debug session
core.assign 1. 2.

; Debug base address for each core
SYStem.CONFIG.COREDEBUG.Base DAP:0x80210000 DAP:0x80310000

; Config access ports
SYStem.CONFIG MEMORYACCESSPORT 0.
SYStem.CONFIG AHBACCESSPORT 0.
SYStem.CONFIG APBACCESSPORT 0.
SYStem.CONFIG DEBUGACCESSPORT 0.
SYStem.CONFIG AXIACCESSPORT 4.

sys.o.WaitReset 1.s

sys.o.EnReset OFF
sys.o.ResBreak OFF

; connect DAP only
SYStem.Mode.Prepare

; Disable vector catch
tronchip.reset
tronchip.set reset off
tronchip.set StepVector off

; Attach and halt
sys.mode.up
if run()
	break.

 

I you cannot progress, maybe ask for direct support to your local ST representative.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Hi @PatrickF  

Thank you for your detailed reply again.

Using the T32 information provided by you, we were able to access the chip. The JTAG clock set was different in our case. and we were able to access the chip when the clock was set to 20MHz.

I apprecaite your timely response.

Thank you again.

 

Hello,

I was wondering if the other cores (Cortex-M33F, Cortex-M0+) on the board are accessed in the same way as the two Cortex-A35 cores.

Is there anything specific required to access them?

When I try to connect, I face an issue that seems related to the cores not being powered or clocked (CPU state: running (core power down)).

Are these cores intended to be debugged? Do you have any idea how I could solve this?

Thanks in advance for your help!

Regards.

Hi @finneass 

other core could be debug using same JTAG port. 
Access port configuration should be adapted (please refer to section "Debug support" of RM0457).

What should be complex in "Development boot" when using 3rd party debugger is that there is also some security settings to be done from CA35 side as related memories required to load code might not be accessible with default security setting (RIF).

Note that Cortex-M33 debug is supported thru CubeIDE / STLINK.

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Hello @PatrickF,

Thank you for your quick response.
I am using Trace32 to connect to the second core.

Connecting to the Cortex-A35 cores works fine, as I can establish a connection without any issues.

However, with the other cores, I get the status "running (core power down)", I reviewed the reference manual, and both the CoreSight ROM table addresses, and the access port configuration appear to be correct.

It seems that a sequence to power up the secondary cores is required, but I have not been able to figure out how to do this.
Do you have an idea on how I can solve this?

Thank you very much for your help, it is highly appreciated!

Best regards.