cancel
Showing results for 
Search instead for 
Did you mean: 

BUG: Setting SIGN_KEY_stm32mp15 leads to error

HLee.21
Associate III

Setting SIGN_KEY_stm32mp15 leads to an error

 

As described here: https://wiki.st.com/stm32mpu/wiki/How_to_perform_Secure_Boot_from_Distribution_package 

Set and adapt these variables:

 

 echo 'SIGN_KEY = "key/stm32mp15/privateKey.pem" ' >> conf/local.conf
 echo 'SIGN_KEY_stm32mp15 = "key/stm32mp15/privateKey.pem" ' >> conf/local.conf 
 echo 'EXTERNAL_KEY_CONF = "1" ' >> conf/local.conf 
 echo 'SIGN_KEY_PASS = "<password of signature key>" ' >> conf/local.conf
 echo 'SIGN_ENABLE = "1" ' >> conf/local.conf 
 echo 'SIGN_TOOL = "<path to STM32MP_SigningTool tools>" '  >> conf/local.conf

DISTRO=openstlinux-weston MACHINE=stm32mp15-eval source layers/meta-st/scripts/envsetup.sh
bitbake st-image-core
ERROR: /st/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.8.bb: [sign-stm32mp] 1 Please make sure to configure "SIGN_KEY_stm32mp13" var to key file.
ERROR: Parsing halted due to errors, see error messages above

It falsely tries to use STM32mp13.

 

Any ideas?

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan SZYMANSKI
ST Employee

Hello @HLee.21 ,
This is something we already faced in the past and I am surprised to see it again on this release. Maybe we missed something at integration step. Thanx for rising this, I will enter an internal ticket to check the point. As a workaround, you can declare the SIGN_KEY_stm32mp13 variable with a key that will not be used in your build. TF-A is just trying to compile for both MP15 and MP13 platforms, but it will not have an impact on your final build.

Sorry for that.

Regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.