2021-01-04 2:27 AM
Hello,
I'm trying to add a python GTK application I created to the startup using systemd.
In order to do so I created the following gatewayservice.service file:
[Unit]
Description=Gateway service
Requires=graphical.target
After=graphical.target
[Service]
Type=idle
ExecStart=/bin/bash /usr/bin/gateway_service.sh
[Install]
WantedBy=multi-user.targetI am able to manually start the service using
systemctl start gatewayserviceBut when I try to add it to startup and reboot it doesn't launch automatically.
I think I'm getting the requirements wrong in the service file but I'm not sure what to put instead.
2021-01-11 1:49 AM
Hi @NRosa.1
Just a quick hint :
The "Demo launcher" application delivered in Starter Package is a GTK application launched by default by systemd.
Cross check how it's done.
Olivier
2021-01-11 1:51 AM
Other hint : change done in Linux FS may require "sync" command to be sure to be record on SDCard for following boot.
Olivier
2021-01-11 2:17 AM
systemctl enable gatewayservice
could check with
systemctl status gatewayservice