Skip to main content
Jungho
Associate II
Dec 15, 2020 12:08 AM UTC
Solved

I'm wondering what's the difference point between STM32MP157C-DK2 and STM32MP157F-DK2?

Hi.

I was going to buy STM32MP157C-DK2 but its status NRND(Not Recommended for New Design). So I think to buy STM32MP157F-DK2.

Are they different point is only a clock(650 or 800) of A7 core? What's the difference?

Thank you.

Best regards.

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
Dec 16, 2020 7:36 AM UTC

I confirm that the major differences are the increased max frequency of the Cortex-A7 cores and the corrections of some HW bugs (Device Rev.Z, see ES0438).

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

Olivier GALLIEN
ST Technical Moderator
Dec 15, 2020 2:38 PM UTC

Hi @Jungho​ ,

STM32MP157F-DK2 is assembled with latest STM32MP15 RevZ cut which is the only one available for new product now.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
PatrickFBest answer
ST Employee
Dec 16, 2020 7:36 AM UTC

I confirm that the major differences are the increased max frequency of the Cortex-A7 cores and the corrections of some HW bugs (Device Rev.Z, see ES0438).

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent