cancel
Showing results for 
Search instead for 
Did you mean: 

Serial communication between linux host and target

medex
Associate

Hi,

 

"I'm using an STM32MP157F-DK2. I'm struggling with the serial connection between my Linux host and my target board (STM32MP157). I'm using the command 'minicom -D /dev/ttyACM0', but I've been waiting for more than 2 hours for the connection to be established, yet it's still not connected.

What can I do to connect to the target device?"

1 ACCEPTED SOLUTION

Accepted Solutions
Nathan_Xi
Associate III

Hi @medex , and welcome to the community!

To connect your device, it's better to use PuTTY, either in ssh or serial. However, the serial connection is the stabler of the two.

Download PuTTY, and connect the ST-LINK port to the USB port of your PC. Find the right serial port, and set the speed to 115200. Finally, click on "Open".

You'll then make a stable connection to your Discovery board.

If this solves your question, it'll be nice of you to click on "Accept as solution".

Good luck!

Nathan Xi

View solution in original post

2 REPLIES 2
Nathan_Xi
Associate III

Hi @medex , and welcome to the community!

To connect your device, it's better to use PuTTY, either in ssh or serial. However, the serial connection is the stabler of the two.

Download PuTTY, and connect the ST-LINK port to the USB port of your PC. Find the right serial port, and set the speed to 115200. Finally, click on "Open".

You'll then make a stable connection to your Discovery board.

If this solves your question, it'll be nice of you to click on "Accept as solution".

Good luck!

Nathan Xi

medex
Associate

Thank you for your prompt and helpful response; it resolved the issue perfectly. Your assistance is greatly appreciated.