2021-12-27 5:23 AM
I have custom stm32mp1 board and when running it as USB mass storage in U-Boot (ums 0 mmc 0), the USB driver is not detected nor by Linux nor by Windows. I am also attaching shematc comparison of eval-board VS my custom board. Also the USB-ORG is working in Engineering mode as DFU device - so I am guessing the soldering and USB pinouts are correct.
Pic.1. Custom board schematics of USB-OTG
2.Pic. Eval-board schematic of USB-OTG.
Solved! Go to Solution.
2022-01-18 8:03 AM
Hi @Arnas Celkys ,
Yes &usbotg_hs phandle can be used on purpose at any level of the dts structure to overwrite some properties set in previous level.
Actually the warning it's to not modified Soc level dtsi.
You are right that in our delivery ST used also a board factorization level (dkx.dtsi or evx.dtsi) you can change since you master what you are doing.
For a custom design I would be more incline to start from a MX generated DTS in order to have a flat board level dts.
Still refer to STM32MP15 device tree - stm32mpu
Olivier
2022-01-03 6:38 AM
Hi @Arnas Celkys ,
I recommend to check your DT and set OTG node according to https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#USB_OTG_node
With ecosystem V3.x, in order to force VBUS and ID pins to be ignored, it should have:
&usbotg_hs {
u-boot,force-b-session-valid;
u-boot,force-vbus-detection;
dr_mode = "peripheral";
};
Btw, the pull-down Rd resistor on CC lines should be 5.1k (but I think 4.7k might not explain why PC did not detect your device as 10% tolerance is allowed)
Regards.
2022-01-04 2:04 AM
Hey, @PatrickF ,
so I followed the 'stm32mp157c-dk2-u-boot.dtsi' include to file 'stm32mp157a-dk1-u-boot.dtsi' located in :<development-packet>/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/arch/arm/dts. Made the following changes:
-----------------------------------------------------------------------------------------------------------------------------------------------------------
&usbotg_hs { //changes made my my, so that OTG-USB does not need Vbus, ID pins
u-boot,force-b-session-valid;
u-boot,force-vbus-detection;
dr_mode = "peripheral";
};
also made a small change to 'stm32mp1.c', to printout the version of u-boot - and indicate that changes were made.
-----------------------------------------------------------------------------------------------------------------------------------------------------------
Then generated new u-boot.img and u-boot-spl.stm32, and uploaded them via USB-as-massstorage to eval-board - board performs as it used to. Then I slid the SD from eval-board to custom board, but still the same problem the masstorage is not detected after ums 0 mmc 0. Infact no USB is detected
STM32MP> ums 0 mmc 0
UMS: LUN 0, dev 0, hwpart 0, sector 0x0, count 0x7400000
Please connect USB cable.
USB cable not detected.
Command exit.
-----------------------------------------------------------------------------------------------------------------------------------------------------------
After making changes to 'stm32mp157a-dk1-u-boot.dtsi' do I need to follow any procedure other than
make stm32mp15_basic_defconfig and DEVICE_TREE=stm32mp157c-dk2 make ?
2022-01-04 7:35 AM
Hi @Arnas Celkys ,
Your process to build and update uboot looks far from the mainstream.
You are on stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17 aka DV3.1.
Uboot-spl (aka basic) is not supported in this version. Do not use stm32mp15_basic_defconfig.
Also BSP partitioning use FIP by default.
Except if you set back to legacy mode the whole image and tsv on SDCard, you can't dd the uboot binary as such.
I recommend to use default configuration and refer to :
How to cross-compile with the Developer Package - stm32mpu
Olivier
2022-01-04 7:56 AM
Thanks, @Community member ,
so just to make sure i understood my mistake fully -
1.1.after saving changes to stm32mp157a-dk1-u-boot.dtsi in <development-packet>/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/arch/arm/dts.
1.2. and optionally making changes to 'stm32mp1.c'
1.3.I should use
make -f $PWD/../Makefile.sdk all UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_trusted_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE="<xxxxxxx-custom>"
----- and this will generate fip-<xxxx-custom>-trusted.bin, and this .bin file is the only file that I need to upload (to fip dir on the pcb) to make changes to U-boot source and DT in U-boot, right?
Also am I correct in assuming all these changes will only affect DT in U-boot? - and therefore if I want to make changes on running OS (for example to use the USB-OTG with no ID or Vbuss pins when Os is runing), I will have to update the DT on the TF-A and/or Kernel? :)
2022-01-05 1:48 AM
also is is per-say I need to enter interactive DDR mode on stm32mp157c-dk2" eval board would this syntax be correct? I do not get any error notifications (when using make ....), but I am not sure if i interpret it correctly
make -f $PWD/../Makefile.sdk all UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_trusted_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE="stm32mp157c-dk2" DDR_INTERACTIVE=1
**************************************************update*****************************************************
when trying to boot it into board i get a fault, and for some reason board is detected as STM32MP157F. It would appear it is loading an old U-boot for some reason, I don't understand why file fip-stm32mp157c-dk2-trusted.bin is re-generated but somehow contains old code...
U-Boot 2020.10-stm32mp-r2 (Dec 22 2021 - 16:30:09 +0200)
CPU: STM32MP157CAC Rev.B
Model: STMicroelectronics STM32MP157F eval daughter on eval mother
Board: stm32mp1 in trusted mode (st,stm32mp157f-ev1)
my custom boot v3-----------------
Board: MB1272 Var2.0 Rev.C-01
DRAM: ERROR: Illegal access to 0xf3afffb0:
ERROR: FAIL_ID = 0x4a0
ERROR: Non-Secure
ERROR: Privilege
ERROR: Read
PANIC at PC : 0x2ffc9b61
Exception mode=0x00000016 at: 0x2ffc9b61
----------------------------------------------------------------------------------------------
this is the make log:
#
# configuration written to .config
#
make[2]: Leaving directory '/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/build/stm32mp15_trusted_defconfig'
make[1]: Leaving directory '/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2'
make[1]: Entering directory '/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2'
make[2]: Entering directory '/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/build/stm32mp15_trusted_defconfig'
GEN ./Makefile
scripts/kconfig/conf --syncconfig Kconfig
CFG u-boot.cfg
GEN include/autoconf.mk
GEN include/autoconf.mk.dep
CFGCHK u-boot.cfg
Using /home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2 as source for U-Boot
/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2 is not clean, please run 'make mrproper'
in the '/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2' directory.
make[2]: *** [/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/Makefile:1813: prepare3] Error 1
make[2]: Leaving directory '/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/build/stm32mp15_trusted_defconfig'
make[1]: *** [Makefile:167: sub-make] Error 2
make[1]: Leaving directory '/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2'
FIP_DEPLOYDIR_UBOOT=/home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/../deploy FIP_DEVICETREE="stm32mp157c-dk2" fiptool-stm32mp
fiptool-stm32mp config:
optee:
bl32 config value: optee
devicetree config: stm32mp157c-dk2
trusted:
bl32 config value: tfa
devicetree config: stm32mp157c-dk2
FIP_DEPLOYDIR_FIP : /home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/../deploy/fip
FIP_DEPLOYDIR_TFA : /home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/../../FIP_artifacts/arm-trusted-firmware/bl32
FIP_DEPLOYDIR_FWCONF: /home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/../../FIP_artifacts/arm-trusted-firmware/fwconfig
FIP_DEPLOYDIR_OPTEE : /home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/../../FIP_artifacts/optee
FIP_DEPLOYDIR_UBOOT : /home/arnas/STM32/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2020.10-stm32mp-r2-r0/u-boot-stm32mp-v2020.10-stm32mp-r2/../deploy
[fiptool] Create fip-stm32mp157c-dk2-optee.bin fip binary into 'FIP_DEPLOYDIR_FIP' folder...
[fiptool] Done
[fiptool] Create fip-stm32mp157c-dk2-trusted.bin fip binary into 'FIP_DEPLOYDIR_FIP' folder...
[fiptool] Done
2022-01-05 5:12 AM
Ok just to make sure that i have left-over configuration I tired to 'make clean' - that did not work so I deleted and re-extracted entire boot source directory.
1.step. Deleted and reextracted boot source .../u-boot-stm32mp-v2020.10-stm32mp-r2.
2.step.
>>make stm32mp15_trusted_defconfig
<<#
<<# configuration written to .config
<<#
3.step.
Configured $FIP_DEPLOYDIR_ROOT and $FIP_DEPLOYDIR_FIP - according to my source locations
4.step.
>>make -f $PWD/../Makefile.sdk all UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_trusted_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE="stm32mp157c-dk2" DDR_INTERACTIVE=1
<< /.../
[fiptool] Create fip-stm32mp157c-dk2-optee.bin fip binary into 'FIP_DEPLOYDIR_FIP' folder...
[fiptool] Done
[fiptool] Create fip-stm32mp157c-dk2-trusted.bin fip binary into 'FIP_DEPLOYDIR_FIP' folder...
[fiptool] Done
5.step.
connect board in mmc mode via USB-ORG and store file fip-stm32mp157c-dk2-trusted.bin from the fip dir in my u-boot source directory and reboot the board.
---------------------------------------------------------------------------------------------------
Also tried using :
>>make clean && make mrproper
before
>>make -f $PWD/../Makefile.sdk all UBOOT_CONFIG=trusted UBOOT_DEFCONFIG=stm32mp15_trusted_defconfig UBOOT_BINARY=u-boot.dtb DEVICETREE="stm32mp157c-dk2" DDR_INTERACTIVE=1
But it still does not entirely clean old models, what should be procedure to clean DT and source of U-boot fully before making changes?
2022-01-05 8:09 AM
Hi @Arnas Celkys ,
Sorry for my previous comment which have confused you.
uboot-spl is supported ONLY for DDR_INTERACTIVE support.
For such please follow strictly the wiki page :
U-Boot SPL: DDR interactive mode - stm32mpu
Else to manage USB mass storage - original question - it's recommended to use default Trusted/ FIP configuration.
In this case generation of proper uboot follow guideline in
How to cross-compile with the Developer Package - stm32mpu
Else, for your point :
1.1.after saving changes to stm32mp157a-dk1-u-boot.dtsi
It's not recommanded to change .dtsi files. All customization might be done at board level ( .dts)
cf warning in page OTG device tree configuration - stm32mpu
And read here to get full structure of DT :
STM32MP15 device tree - stm32mpu
Olivier
2022-01-06 12:15 AM
Thanks, @Community member
Could you help me out with this issue:
First I would like to ended DDR interactive mode using "stm32mp15_trusted_defconfig" rather then "stm32mp15_basic_defconfig".
So I proceed like so :
>>make clean && make mrproper
<<
CLEAN scripts/basic
CLEAN scripts/kconfig
CLEAN .config
>>make stm32mp15_trusted_defconfig
<<
#
# configuration written to .config
#
>>DEVICE_TREE=stm32mp157c-dk2 DDR_INTERACTIVE=1 make
<<
CC drivers/core/simple-bus.o
CC drivers/core/dump.o
CC drivers/core/regmap.o
CC drivers/core/syscon-uclass.o
CC drivers/core/of_extra.o
CC drivers/core/ofnode.o
drivers/core/ofnode.c:239:6: error: redefinition of ‘ofnode_is_enabled’
239 | bool ofnode_is_enabled(ofnode node)
| ^~~~~~~~~~~~~~~~~
drivers/core/ofnode.c:229:6: note: previous definition of ‘ofnode_is_enabled’ was here
229 | bool ofnode_is_enabled(ofnode node)
| ^~~~~~~~~~~~~~~~~
make[2]: *** [scripts/Makefile.build:266: drivers/core/ofnode.o] Error 1
make[1]: *** [scripts/Makefile.build:419: drivers/core] Error 2
make: *** [Makefile:1780: drivers] Error 2
and get this wierd error of double definition of 'ofnode_is_enabled', was my 'ofnode.c' file corrupted? Should I re-download it?
----------------------------------------------------------------------------------------------------------
Also after successful "DEVICE_TREE=stm32mp157c-dk2 DDR_INTERACTIVE=1 make", should I upload u-boot-spl.stm32 and u-boot.img to /fip + /fsbl1 + /fsbl2 ? Or should I follow different steps?
It does not define it in U-Boot SPL: DDR interactive mode - stm32mpu
----------------------------------------------------------------------------------------------------------
2022-01-06 1:40 AM
Hi @Arnas Celkys
DDR_INTERACTIVE=1 is only supported in "stm32mp15_basic_defconfig" not with "stm32mp15_trusted_defconfig" .
----------------------------------------------------------------------------------------------------------
Also after successful "DEVICE_TREE=stm32mp157c-dk2 DDR_INTERACTIVE=1 make", should I upload u-boot-spl.stm32 and u-boot.img to /fip + /fsbl1 + /fsbl2 ? Or should I follow different steps?
It does not define it in U-Boot SPL: DDR interactive mode - stm32mpu
----------------------------------------------------------------------------------------------------------
Yes it is. See chapter 3 Load the SPL into embedded RAM
You can ignore FIP in this case. Uboot spl will come in fsbl partition.
Olivier