cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP257F-EV1 STLinux Packages: Serial command line

mfny
Associate III

Hello,

I am wondering can the ST Linux Starter Package(or indeed any of the STLinux packages) be interacted with via a command line via serial port and if so how would this be set up ? as the additional display for this board is unavailable to me.

1 REPLY 1
PatrickF
ST Employee

Hi @mfny 

for sure, the Starter Package console is available thru STLINK. This is the main control interface to Linux (for tests or install additional packages).

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Let%27s_start/Unpack_the_STM32MP257x-EV1_board#Board_connections

Just connect USB Type-C CN21 to a PC and you will have 2 x VCP available (one for Cortex-A35 Console, the second optional for Cortex-M33 console).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here