2025-05-21 4:48 AM - last edited on 2025-05-21 4:53 AM by Peter BENSCH
Hi there,
I am working with the STM32MP135F-DK microprocessor and have already designed the user interface in Figma. Now, I would like to move forward with developing this UI.
Which tool should I use to implement the UI on the STM32MP135F-DK?
If I choose to use Qt Creator, can I use the open-source version for a client project, or would I need a commercial license? Are there any legal limitations or issues I should be aware of?
Thanks in advance for your guidance.
2025-05-22 7:59 AM
2025-06-25 5:10 AM
Hi,
MP135 indeed supports several UI frameworks.
You can consider these solutions:
- Qt with open-source version:
https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package
- LVGL:
https://wiki.st.com/stm32mpu/wiki/How_to_build_LVGL_applications_using_STM32CubeIDE
- STM TouchGFX package:
BR,
Philippe.