2020-09-25 9:04 AM
When building a distro for our custom board with a STM32MP153AAC, u-boot-stm32mp fails to build when UBOOT_CONFIG is set to "basic". We would like to do a ddr3 test, this is the reason for the config.
Here is the relevant section from conf/machine/stm32mp1-raichu-v2.conf file
###########################################################################
#
# User machine customization sections
#
###########################################################################
# Boot Scheme
# =========================================================================
BOOTSCHEME_LABELS += "trusted"
# WORKAROUND to generate U-BOOT SPL for DDR Tuning tools usage
UBOOT_CONFIG += "basic"It seems that the dsi block is defined in arch/arm/dts/stm32mp157.dtsi, but we have a stm32mp153, and the device tree generated by CubeMX only includes stm32mp153.dtsi. So obviously, this isn't going to work:
2020-11-02 1:14 AM
Hi
I too don't see a patch. I see a 98.6MB tar file attached to your post. Would it be possible to post a diff (.patch file) instead?
Many thanks
2020-11-04 8:53 AM
Hi @AMurr.2282 ,
Sorry !
Don't know what's going on ..
the patch is very simple actually :
diff --git a/arch/arm/dts/stm32mp15-no-scmi.dtsi b/arch/arm/dts/stm32mp15-no-scmi.dtsi
index 4837b34..064fd56 100644
--- a/arch/arm/dts/stm32mp15-no-scmi.dtsi
+++ b/arch/arm/dts/stm32mp15-no-scmi.dtsi
@@ -61,6 +61,10 @@
clocks = <&rcc CRYP1>;
resets = <&rcc CRYP1_R>;
};
+
+ dsi: dsi@5a000000 {
+ clocks = <&rcc DSI_K>, <&clk_hse>, <&rcc DSI_PX>;
+ };
};
mlahb {
@@ -100,10 +104,6 @@
clocks = <&rcc DDRPERFM>, <&rcc PLL2_R>;
};
-&dsi {
- clocks = <&rcc DSI_K>, <&clk_hse>, <&rcc DSI_PX>;
-};
-
&gpioz {
clocks = <&rcc GPIOZ>;
};Olivier
2020-11-05 3:56 AM
Thanks! I applied the patch and U-Boot SPL compiled successfully.
I tried to load bootloader/u-boot-spl.stm32 onto the target board using STM32CubeMX DDR Test Suite and now I am getting the following output on serial:
U-Boot SPL 2020.01-stm32mp-r1 (Nov 05 2020 - 11:15:33 +0000)
Model: STMicroelectronics custom STM32CubeMX board
RAM: DDR3-DDR3L 16bits 533000Khz
DDR invalid size : 0x0, expected 0x10000000
DRAM init failed: -22
### ERROR ### Please RESET the board ###It looks like PMIC isn't enabling DDR3 VDD, VTT or VREF because I measure 0V.
Any idea how I can fix this?