2023-02-06 6:11 AM
Trying to compile wpe-browser from meta-wpewebkit and during building cog I'm getting error:
https://github.com/Igalia/meta-webkit/issues/446
It seems that gcnano-userland-multi-binary-stm32mp provides gbm.h which clash with one from cog.
I've resolved it by:
`GPU_USERLAND_LIBRARIES_WAYLAND = "mesa"` adding to local.conf
and also by adding append for gcnano-userland-multi-binary-stm32mp.bbappend
with content:
`GCNANO_PACKAGECONFIG:remove = "gbm"` but when I start wpe browser it display just white background and nothing more.
Thanks.
2023-02-09 1:56 AM
Hi @MBeli.1
What is your OpenSTLinux ecosystem version? 4.1?
Do you select the kirkstone branch from the meta-webkit layer?
Best regards,
--JM
2023-02-09 2:33 AM
@Jean-Marc B Exactly. OpenSTLinux is 4.1 and on meta-webkit I use kirkstone branch.
Thanks.
2023-02-10 12:34 AM
Hi @MBeli.1
The issue you related about no page displayed by the browser may be related to this issue which seems to be still active (last post 3 weeks ago):
https://github.com/Igalia/meta-webkit/issues/184
It seems to me the problem is based on Qt integration / version.
Best regards
--JM
2023-02-10 12:41 AM
@Jean-Marc B ok thanks, maybe yes. But how about this error:
```Compiling cog for stm32 platform kirkstone branch getting following :
cog/0.14.1-r0/cog-0.14.1/platform/drm/cog-drm-modeset-renderer.c:110:1: error: conflicting types for 'get_drm_fd'; have 'int(CogDrmModesetRenderer *)'
110 | get_drm_fd(CogDrmModesetRenderer *self)
| ^~~~~~~~~~
In file included from /data/projects/test/yocto/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/cog/0.14.1-r0/cog-0.14.1/platform/drm/cog-drm-modeset-renderer.c:11:
/data/projects/test/yocto/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/cog/0.14.1-r0/recipe-sysroot/usr/include/gbm.h:246:1: note: previous declaration of 'get_drm_fd' with type 'int(void)'
246 | get_drm_fd(void);
| ^~~~~~~~~~
```
Thanks.
2023-02-14 12:05 AM
Hi @MBeli.1
It is hard to fix the compilation error as the library and the application define the same function. The application here does not expect this function provided by the current libgdm implementation.
Your work-around is correct. However, you can use MESA to drive the GPU but not in commercial products because of the end-user license agreement (EULA).
Best regards,
--JM