2025-01-14 8:22 PM
Hi Team,
There are two version of OSTL i.e. v4.0.0 STM32 MPU OpenSTLinux release note - v4.0.0 - stm32mpu-ecosystem-v4 and v4.1.0 STM32 MPU OpenSTLinux release note - v4.1.0 - stm32mpu-ecosystem-v4. what is difference between them both are at 5.15.x kernel and using Kirkstone?
Is OSTL v4.1.0/v4.1.1/v4.1.2 backward compatible with v4.0.0/v4.0.1/v4.0.2? @OlivierK
Thank you.
2025-01-14 11:18 PM
Hi @GChin.1 ,
Release 4.1 is a maintenance release of the 4.0 ecosystem release using same Yocto (Kirkstone) and Kernel version (5.15)
Differences are listed in STM32 MPU OpenSTLinux release note - v4.1.0 - stm32mpu-ecosystem-v4
Even if backward compatibility may exist, we always recommend using all components version from the same version, as validated by ST.
Note that 4.x releases are no more supported by ST and so not recommended for new design.
Please use the latest V6
STM32 MPU ecosystem release note - stm32mpu
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.