2024-12-25 4:28 AM
I have both Board "stm32mp257F-dk - F-ev"
I try to install chromium on the STM32MP2 , and Successfully installed chromium ,
I try to play video on YouTube it is to lagging , smoothly play on 360p only, without YouTube i treid different method to play video on chromium. but also the output same,
is there any thing to reslove this issues?
My project based of Web display with high resolution video upto 1080p60 fps on HDMI .
please give me the update on this, can my project work on this board.
2025-01-27 3:56 AM
Hi,
today Chromium does not support natively our hardware video decoder on MP2.
We are in the phase to integrate adaptation so that we can get benefit of our hardware acceleration.
It should probably come out in the second half of 2025.
If you need to play high resolution streams, please use gstreamer.
Philippe.