Question
How to initialize USB_OTG_FS in CubeMX?
Hello,
I am currently initializing my STM32MP157CAC3 (TFBGA361) with CubeMX.
The processor's datasheet lists USB_OTG_FS functionality as additional functions on PA11 / PA12 but there is no such selection inside CubeMX.
In general, there is no USB_OTG_FS functionality listed (only USB_OTG_HS, which I can't use because the pins are already used by USB_HS2).
Is it possible to configure this peripheral inside CubeMX?
MPU: STM32MP157CAC3
CubeMX Version: 5.6.0.202002181639
MPU Firmware Package: V1.2.0