2020-12-11 2:05 AM
Hello
I am getting the following error after trying to build the image
The rootfs size 5956484(K) exceeds IMAGE_ROOTFS_MAXSIZE: 763904(K)
and I don't find anything related to this problem apart from this line that should be implemented in the local.conf file:
MENDER_STORAGE_TOTAL_SIZE_MB=....
Will this solve my problem? If not how do I solve this problem please I am a beginner with yocto.
I want to use the maximum space that I can so that this error won't come again. I will add a lot of packages and modules after so please tell me if there is a default size to apply.
Thank you
2020-12-15 7:46 AM
Hello SigmaPrime (Community Member)
Your rootfs partition size seems a bit large... almost 6GB! are you sure?
Do you have this error when creating the image from the script create_sdcard_from_flashlayout.sh? if so 768MB is the defaut size set for rootfs in the script.
to increase the rootfs size, you can just change the value DEFAULT_ROOTFS_PARTITION_SIZE according to your needs.
Hope it helps.
Olivier