2024-10-31 1:40 AM
Hello everyone,
I am trying to migrate a project for the STM32MP151C from dunfell to kirkstone.
The versions of the main components I am using are the following:
| Component | Version | 
| tf-a-stm32mp | v2.6-stm32mp-r2.2 | 
| optee-os-stm32mp | v3.16.0-stm32mp-r2.2 | 
| u-boot-stm32mp | v2021.10-stm32mp-r2.2 | 
| linux-stm32mp | v5.15.145-stm32mp-r2.2 | 
I used a given .ioc file with a newer version of STM32CubeMX (v6.8.0 - openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23) to re-generate the devicetrees and added the custom changes from the old devicetrees (see devicetrees attached).
Eventually during boot following error occurs:
I/TC: Primary CPU switching to normal world boot
D/TC:0   tee_entry_exchange_capabilities:100 Asynchronous notifications are disabled
D/TC:0   tee_entry_exchange_capabilities:112 Dynamic shared memory is enabled
D/TC:0 0 core_mmu_xlat_table_alloc:513 xlat tables used 4 / 4
D/TC:? 0 tee_ta_init_pseudo_ta_session:296 Lookup pseudo TA a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
D/TC:? 0 tee_ta_init_pseudo_ta_session:309 Open PTA-SCMI
D/TC:? 0 tee_ta_init_pseudo_ta_session:326 PTA-SCMI : a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
D/TC:? 0 tee_ta_close_session:514 csess 0x2ffec928 id 1
D/TC:? 0 tee_ta_close_session:533 Destroy session
D/TC:? 0 tee_ta_init_session_with_context:609 Re-open TA a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
D/TC:? 0 tee_ta_close_session:514 csess 0x2ffec928 id 1
D/TC:? 0 tee_ta_close_session:533 Destroy session
D/TC:? 0 tee_ta_init_session_with_context:609 Re-open TA a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
D/TC:? 0 tee_ta_close_session:514 csess 0x2ffec928 id 1
D/TC:? 0 tee_ta_close_session:533 Destroy session
D/TC:? 0 tee_ta_init_session_with_context:609 Re-open TA a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
D/TC:? 0 tee_ta_close_session:514 csess 0x2ffec928 id 1
D/TC:? 0 tee_ta_close_session:533 Destroy session
D/TC:? 0 tee_ta_init_session_with_context:609 Re-open TA a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
D/TC:? 0 tee_ta_close_session:514 csess 0x2ffec928 id 1
D/TC:? 0 tee_ta_close_session:533 Destroy session
D/TC:? 0 tee_ta_init_pseudo_ta_session:296 Lookup pseudo TA 94cf71ad-80e6-40b5-a7c6-3dc501eb2803
D/TC:? 0 tee_ta_init_pseudo_ta_session:309 Open bsec.pta
D/TC:? 0 tee_ta_init_pseudo_ta_session:326 bsec.pta : 94cf71ad-80e6-40b5-a7c6-3dc501eb2803
E/TC:0
E/TC:0   Core prefetch-abort at address 0x300135a8 (translation fault)
E/TC:0    fsr 0x00000207  ttbr0 0x2ffdf000  ttbr1 0x00000000  cidr 0x0
E/TC:0    cpu #0          cpsr 0x600001f3
E/TC:0    r0 0x2ffec588      r4 0x2ffec588    r8 0x00000000   r12 0x00000020
E/TC:0    r1 0x00000200      r5 0x00000024    r9 0xcdf0ee90    sp 0x2ffe10b0
E/TC:0    r2 0xdededede      r6 0x00000000   r10 0x0badc0de    lr 0x2ffca2b1
E/TC:0    r3 0x300135a9      r7 0x00000000   r11 0xe320f000    pc 0x300135a8
E/TC:0   TEE load address @ 0x2ffc0000
E/TC:0   Call stack:
E/TC:0    0x300135a8
E/TC:0   Panic 'abort outside thread context' at ?:0
E/TC:0   TEE load address @ 0x2ffc0000
E/TC:0   Call stack:
E/TC:0    0x2ffc2269
E/TC:0    0x2ffca375
E/TC:0    0x2ffc1e6f
E/TC:0    0x2ffc0b24
Has somebody an idea why this error occurs and/or how I can fix it?
Any help would be greatly appreciated :)
Solved! Go to Solution.
2024-10-31 7:14 AM
Hi @dhk112 ,
I noticed you have 256MB DDR budget which can be quite complex to manage when using OPTEE.
We generate a guideline here How to configure a 256MB DDR mapping from STM32 MPU Distribution Package - stm32mpu-ecosystem-v4
Olivier
2024-10-31 3:59 AM - edited 2024-10-31 4:00 AM
Hi @dhk112
Before addressing technical point I would first understand/challenge your migration strategy.
What reason to migrate and why only on kirkstone (V4.x) which is close to end of maintenance ?
I would rather recommend to move to latest V5.1 / openstlinux-6.1-yocto-mickledore-mpu-v24.06.26, or even, if you can wait few weeks, the coming V6 ( Scarthgap kernel 6.6 ).
Else your migration strategy looks good, by generating DTS backbone with relevant MX version and porting the custom change.
Maybe a review/comparison against reference device tree generated by CubeMX for our evaluation board may help to catch some hidden policy change that may explain some issues.
Hope it help
Olivier
2024-10-31 6:11 AM
Hi Oliver,
thanks for the reply.
I am aware that kirkstone is already close to end of maintenance, but for the moment this project should be ported to kirkstone first and later on to a newer version for project-related reasons that are not relevant here.
I already compared a lot to the device trees of evaluation boards but I can not figure out what might be wrong with my devicetrees.
What parts of the device tree (or possibly other build configuration) could be related to this error?
Best regards
2024-10-31 7:14 AM
Hi @dhk112 ,
I noticed you have 256MB DDR budget which can be quite complex to manage when using OPTEE.
We generate a guideline here How to configure a 256MB DDR mapping from STM32 MPU Distribution Package - stm32mpu-ecosystem-v4
Olivier
2024-11-03 11:40 PM
Hi Oliver,
thanks for the hint! I will look into it and report back if it could solve the issue.
Best regards,
dhk
2024-11-04 7:21 AM
Hi Oliver,
this solved my problem, thanks again!
Best regards,
dhk
2024-11-04 7:33 AM
Great ! Thanks for feedback !
Olivier