2020-10-15 1:59 PM
Hey Team,
I'm trying to get through a board bring up with the STM32MP157 silicon ver 2001 marked with a Z.
We are trying to boot the system from the on board eMMC (Insignis Technology Corp P/N: NSEC53K008-IT 8GB eMMC ) and are having issues. We have configured the boot pins correctly and also confirmed emmc hardware connections are correct by successfully reading and writing the emmc from linux while booting from the SD card.
There seems to be a lack of documentation on how to configure the eMMC and partition it. Is there any specific partition scheme that needs to be followed for the MP1?
And link to an app note that documents how to configure the eMMC via STM32Programmer or UBoot for booting would be extremely helpful.
Jason
2020-10-16 12:08 AM
Hello.
We have too issue with emmc but now, it's ok !
look at these post:
"EMMC Questions " on ST forum
and
"https://www.emcraft.com/som/stm32mp1/booting-linux-from-emmc"-->coolest one
"https://community.st.com/s/question/0D50X0000BiBhHQSQ0/stm32mp153a-failed-to-boot-from-emmc"
After that, we program the emmc by starting on a sdcard, mounting emmc partition on linux, and copy ext4 file on the it.(usb key->stmp32mp1 board->emmc
well it works. i first partition emmc from uboot, and after that i get an "exported partition" that i can use on others board.
Be aware you have to modify a register from uboot / linux:
using: mmc boot part enable (+config) in user domain linux
or
mmc partconf (+config) in uboot
good luck