cancel
Showing results for 
Search instead for 
Did you mean: 

bitbake error

Sharan
Senior II
NOTE: Started PRServer with DBfile: /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, Address: 127.0.0.1:35035, PID: 9978
Loading cache: 100% |                                                                                                                                                   | ETA:  --:--:--
Loaded 0 entries from dependency cache.
NOTE: /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb: ENABLE_PARTITIONS_IMAGE not enabled
Parsing recipes: 100% |##################################################################################################################################################| Time: 0:02:31
Parsing of 2868 .bb files complete (0 cached, 2868 parsed). 4596 targets, 530 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION           = "2.4.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "ubuntu-24.04"
TARGET_SYS           = "arm-ostl-linux-gnueabi"
MACHINE              = "stm32mp1"
DISTRO               = "openstlinux-weston"
DISTRO_VERSION       = "4.2.4-snapshot-20241010"
TUNE_FEATURES        = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU           = "hard"
DISTRO_CODENAME      = "mickledore"
ACCEPT_EULA_stm32mp1 = "1"
GCCVERSION           = "12.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
meta-python          
meta-oe              
meta-gnome           
meta-multimedia      
meta-networking      
meta-webserver       = "HEAD:aa5e8edabbc414d8ec1b2ad63c8743c7baf99626"
meta-st-stm32mp      = "HEAD:1f152e07019dc06fd331b4926ec7e76ceae3d259"
meta-st-openstlinux  = "HEAD:2636960b2bead3d1cb294e378e2b06ef8997189e"
meta                 = "HEAD:23b5141400b2c676c806df3308f023f7c04e34e0"

NOTE: Fetching uninative binary shim http://downloads.yoctoproject.org/releases/uninative/4.3/x86_64-nativesdk-libc-4.3.tar.xz;sha256sum=1c35f09a75c4096749bbe1e009df4e3968cde151424062cf4aa3ed89db22b030 (will check PREMIRRORS first)
WARNING: Your host glibc version (2.39) is newer than that in uninative (2.38). Disabling uninative so that sstate is not corrupted.
Initialising tasks: 100% |###############################################################################################################################################| Time: 0:00:11
Sstate summary: Wanted 3246 Local 0 Mirrors 0 Missed 3246 Current 0 (0% match, 0% complete)
NOTE: Executing Tasks
ERROR: PermissionError: [Errno 1] Operation not permitted

During handling of the above exception, another exception occurred:

Traceback (most recent call last):
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/bin/bitbake-worker", line 275, in child
    bb.utils.disable_network(uid, gid)
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/lib/bb/utils.py", line 1693, in disable_network
    with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted

ERROR: Task (/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-devtools/gcc/gcc-source_12.3.bb:do_rm_work) failed with exit code '1'
ERROR: PermissionError: [Errno 1] Operation not permitted

During handling of the above exception, another exception occurred:

Traceback (most recent call last):
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/bin/bitbake-worker", line 275, in child
    bb.utils.disable_network(uid, gid)
  File "/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/bitbake/lib/bb/utils.py", line 1693, in disable_network
    with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted

ERROR: Task (/home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_6.1.bb:do_rm_work) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6 tasks of which 0 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 3 seconds

Summary: 2 tasks failed:
  /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-devtools/gcc/gcc-source_12.3.bb:do_rm_work
  /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_6.1.bb:do_rm_work
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code.
1 ACCEPTED SOLUTION

Accepted Solutions
PPAGE.13
ST Employee

Hi,

as I said to you on another post, you need to move to Ubuntu 22.04 or 20.4.

Ubuntu 24 has not been tested.

https://wiki.st.com/stm32mpu/wiki/PC_prerequisites

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
PPAGE.13
ST Employee

Hi,

as I said to you on another post, you need to move to Ubuntu 22.04 or 20.4.

Ubuntu 24 has not been tested.

https://wiki.st.com/stm32mpu/wiki/PC_prerequisites

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sharan
Senior II

i have moved to ubuntu 22.04 and i have downloaded distribution package but i cant find

FlashLayout_sdcard_stm32mp157d-dk1-optee.tsv  

Ok,  so almost 6 months later and we still can't use Ubuntu 24?  It is 2025.

Is this on this todo list?

Sharan
Senior II

yes u cant use ubuntu 24 as it has been tested with only  ubuntu 22.04