cancel
Showing results for 
Search instead for 
Did you mean: 

Power Supply for STM32MP157C-DK2

SChau.2062
Associate III

Hello,

We would like to setup the STM32MP157C-DK2 board. But we couldn't find any information related to the recommended power supply.

Could you please suggest us that which Power Supply 5V/3A adapter or connector should we use? It would be great if you can provide us link to purchase the power supply adapter or connector because the power supply is not delivered.

We tried to use HUAWEI superfast power supply adapter but we faced this problem: https://community.st.com/s/question/0D50X0000Bftpj3SQA/cant-able-to-populate-the-target-and-boot-the-image-on-stm32mp157cdk2

Thanking you!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Power supply is usually not an issue if it could provide more than 1A (more current are required only for intensive usage, but also 2A are provisioned to supply the 4 x USB Type-A of the DK2 with up to 500mA each).

With some supplies, you could see the red led blinking one or two times to indicates that the Type-C supply has not been detected as 3A (could be also because it is not 100% Type-C compliant or using a Type-A <-> Type-C cable). This is a warning only and does not stop the boot process.

Some supplies are even not detected at all as a Type-C, then the red led is kept light and the boot process is stopped.

Here are some list of tested supplies (without any ST endorsement as model could change without notice):

0690X00000AsSGZQA3.jpg

For details on console message and red LED blinking signification, see Populate the target and boot the image.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Power supply is usually not an issue if it could provide more than 1A (more current are required only for intensive usage, but also 2A are provisioned to supply the 4 x USB Type-A of the DK2 with up to 500mA each).

With some supplies, you could see the red led blinking one or two times to indicates that the Type-C supply has not been detected as 3A (could be also because it is not 100% Type-C compliant or using a Type-A <-> Type-C cable). This is a warning only and does not stop the boot process.

Some supplies are even not detected at all as a Type-C, then the red led is kept light and the boot process is stopped.

Here are some list of tested supplies (without any ST endorsement as model could change without notice):

0690X00000AsSGZQA3.jpg

For details on console message and red LED blinking signification, see Populate the target and boot the image.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.