2024-09-09 10:25 PM
Hi
i am struggling in how to boot from the EMMC not from the SD card , i used the custom board where my emmc is connected to SDMMC2 port , i did changes into the device tree i enable the sdmmc2, but i do not know how to boot from the emmc ?,
actually my custom board based on the (STM32MP157D -Dk1), there is no EMMC but in custom board i added the emmc with SDMMC2 channel, so please help me out this situation how to boot ,
please Ignor my basic question i am the frasher and doing own self, i need your support for learn.
Solved! Go to Solution.
2024-09-10 11:29 PM
did you set the BOOT pins to eMMC (b010)? Boot_device_selection_on_STM32MP1_series
see also Boot_from_e-MMC
Regards.
2024-09-10 11:29 PM
did you set the BOOT pins to eMMC (b010)? Boot_device_selection_on_STM32MP1_series
see also Boot_from_e-MMC
Regards.
2024-09-13 3:43 AM
hi @PatrickF ,
Actually, my boot1 pin is connected to the ground, it is always present as 0 as like (stm32mp157f-dk2),
i am attaching the custom board of bootpin, connection
2024-09-13 5:23 AM
Hi,
until you fix your PCB to have correct BOOT pins allowing to select the memory you implemented (there is no eMMC on STM32MP157x-DK board), you might have a solution using OTP3 primary_boot_source field to the value 3.
Regards,
2024-09-13 10:37 PM
l done the changes into my custom board hardware and setup the boot pin( 0 1 0 ).
I removed the wifi configuration from the DTS file.
####### stm32mp157-discovery DTS##########################################
&sdmmc2 {
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc2_b4_pins_a>;
pinctrl-1 = <&sdmmc2_b4_od_pins_a>;
pinctrl-2 = <&sdmmc2_b4_sleep_pins_a>;
non-removable;
st,neg-edge;
bus-width = <4>;
vmmc-supply = <&v3v3>;
mmc-pwrseq = <&wifi_pwrseq>;
#address-cells = <1>;
/* brcmf: bcrmf@1 {#size-cells = <0>;
status = "okay";
reg = <1>;
compatible = "brcm,bcm4329-fmac";
interrupt-parent = <&gpiod>;
interrupts = <0 IRQ_TYPE_LEVEL_HIGH>; /* WL_HOST_WAKE */
interrupt-names = "host-wake";
}; */
};
######################## pin controll ##############################################
sdmmc2_b4_pins_a: sdmmc2-b4-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
<STM32_PINMUX('A', 9, AF10)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 5, AF9)>, /* SDMMC2_D6 */
<STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
};
sdmmc2_b4_od_pins_a: sdmmc2-b4-od-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
<STM32_PINMUX('A', 9, AF10)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
pins3 {
pinmux = <STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-disable;
drive-open-drain;
slew-rate = <1>;
};
};
sdmmc2_b4_sleep_pins_a: sdmmc2-b4-sleep-0 {
pins {
pinmux = <STM32_PINMUX('A', 8, ANALOG)>, /* SDMMC2_D4 */
<STM32_PINMUX('A', 9, ANALOG)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 3, ANALOG)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, ANALOG)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 14, ANALOG)>, /* SDMMC2_D0 */
<STM32_PINMUX('B', 15, ANALOG)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, ANALOG)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 3, ANALOG)>, /* SDMMC2_CK */
<STM32_PINMUX('E', 5, ANALOG)>, /* SDMMC2_D6 */
<STM32_PINMUX('G', 6, ANALOG)>; /* SDMMC2_CMD */
};
};
########################### ##################################################
again i boot the SD card and check the hardware configuration.
Hit any key to stop autoboot: 0
STM32MP> mmc list
STM32 SD/MMC: 0 (SD)
STM32MP>
STM32 SD/MMC: 0 (SD)
STM32MP>
STM32 SD/MMC: 0 (SD)
STM32MP>
STM32 SD/MMC: 0 (SD)
STM32MP>
STM32 SD/MMC: 0 (SD)
STM32MP>
STM32 SD/MMC: 0 (SD)
STM32MP>
2024-09-13 10:38 PM
hi @PatrickF
please check my reply i did not understand.