cancel
Showing results for 
Search instead for 
Did you mean: 

How do I control STM32MP157 Cortex-M4-only reset signal using a Segger J-Link or J-Trace?

Spamfast
Associate II

I've asked Segger but I was wondering if anyone knows how to get a Segger J-Link/Trace to put only the M4 core on an STM32MP157 into reset and bring it back out?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
OlivierK
ST Employee

Hi,

You should indeed ask Segger directly, It seems J-link SDK, https://www.segger.com/products/debug-probes/j-link/technology/j-link-sdk/

can send reset command from the cmd prompt.

It should works for debug the CortexM4, with the STM32MP157 board set in Engineering boot mode (to connect only to the Cortex M4 through JTAG).

Some related topics also:

https://forum.segger.com/index.php/Thread/7557-ABANDONED-Can-t-connect-to-M4-core-of-STM32MP1-STM32MP157/