cancel
Showing results for 
Search instead for 
Did you mean: 

FAQ: Possible communication failure between STLINK-V3 and some recent computers

FBL
ST Employee

While the STLINK-V3 is compliant with USB 2.0 and exhibits reliable USB performance across various platforms since several years, the USB communication may fail between an STLINK-V3 and some recent computers. 

1. Root cause

The root cause comes from the interoperability issues of a eUSB2 to USB 2.0 High-Speed repeater used on certain recent computers. This repeater doesn’t respect the original USB2 specification. As of September 2024, USB-IF has published a new release of the Embedded USB2 (eUSB2) Physical Layer Supplement to the USB Revision 2.0 Specification (Rev.1.2) on their website. This release now includes a new ECN entitled “Repeater HS SYNC Forward”, addressing the interoperability aspect for future devices.

2. Mitigation

To mitigate potential USB communication failures between your host computer and your STLINK-V3 device (this applies to standalone STLINK-V3SET, STLINK-V3MINIE, STLINK-V3MODS probes, and to embedded STLINK-V3 on Nucleo boards and Discovery kits), we suggest the following tested workarounds:

  1. Try to connect to another USB Type-C® port on your computer if available. Alternatively, using a USB Type-A port of your computer usually solves the issue.
  2. Connect the STLINK-V3 via an external USB High-Speed hub to the USB Type-C® port of your host computer (tested hub reference: Anker332 5in1).
  3. Use a different standalone probe to connect to your target board: ST-LINK/V2, STLINK-V3PWR, Segger J-Link.

Our team is actively exploring additional solutions to this issue. We apologize for any inconvenience this may cause, and we appreciate your understanding as we work to resolve this matter.

 

Comments

In affected cases, would the ST-Link show up in Windows Device Manager (or equivalent on other systems)?

 

Ref: https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

MKori.1
Associate III

Is the issue with the missing full-speed implementation resolved? Previous it wasn't possible to connect a STLink-V3 via an USB-2 Full-Speed (not High-Speed) Isolator as the driver interface implementation was just an empty shell.


Please also see:
https://community.st.com/t5/stm32-mcus-boards-and-hardware/failed-to-connect-to-stlink-v3-using-a-usb-isolator/m-p/273483/highlight/true#M9452

davetoaster
Associate

This issue also affects any product that uses the STM32F7 for USB 2.0 HS with the built-in PHY (not just STLINK probes).

That means that the STM32F7's USB HS peripheral simply doesn't work with recent Apple Macs. Would love to hear if there's a workaround for this!

FBL
ST Employee

Hi @davetoaster 

Unfortunately, no software workaround for that interoperability issue with the eUSB repeaters on F7 family.

Version history
Last update:
‎2024-10-29 3:07 AM
Updated by:
Contributors