cancel
Showing results for 
Search instead for 
Did you mean: 

X-Cube-Matter cannot be compiled with MDK Arm

AkihiroN
Senior

I am developing using X-Cube-Matter v1.4.0.
I imported the BLE_Ota project onto MDK Arm and built it, but the following error occurred and I was unable to compile it.

../Core/Src/app_entry.c(28): warning: In file included from...
../STM32_WPAN/app\app_thread.h(30): error: 'stm32wbxx_core_interface_def.h' file not found
30 | #include "stm32wbxx_core_interface_def.h"

 

Please tell me the cause.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @AkihiroN 

BLE_OTA app is part of X-Cube-Matter OTA sample with SBSFU and Matter SDK. It has been built under CubeIDE. It may be just porting issue. Could you please test it using CubeIDE. And as a recommendation, it is better to use the last version of the STM32CubeIDE for any use case on the X-Cube-Matter.

Best Regards.

STTwo-32

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
STTwo-32
ST Employee

Hello @AkihiroN 

I've escalated this behavior internally to be checked (under internal ticket number 207666). I will be back to you ASAP.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STTwo-32
ST Employee

Hello @AkihiroN 

BLE_OTA app is part of X-Cube-Matter OTA sample with SBSFU and Matter SDK. It has been built under CubeIDE. It may be just porting issue. Could you please test it using CubeIDE. And as a recommendation, it is better to use the last version of the STM32CubeIDE for any use case on the X-Cube-Matter.

Best Regards.

STTwo-32

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @STTwo-32 

Thank you for your confirmation. I understand.

However, if possible in the next update, I would appreciate it if you could consider making it compatible with Keil MDK Arm as well.

 

Best Regards.

I will escalate your request to review this possibility.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you. Please close this matter.

Best Regards.

X-CUBE-MATTER version 1.4.1 has been released.
Does this version support SDKs other than STM32CubeIDE, such as Keil MDK Arm?

Also, is it possible to use version 1.4.1 on a Mac environment?
I tried building STM32WB5MM_DISCO_2_Images_SECoreBin on STM32CubeIDE, but the build failed.