cancel
Showing results for 
Search instead for 
Did you mean: 

Wireless Copro binaries

AWack
Senior

Hi,

I´m just starting with Matter over Thread (with the Lighting-App from github).

I´m  a little bit confused which binary is for which purpose, because the file various file names:

- BLE_Thread_dynamic / static (from STM32Cube_FW_WB_V1.19.0)

- Thread_xxx (from STM32Cube_FW_WB_V1.19.0)

- BLE_Thread_ForMatter (from the github example)

 

Especially for me the difference between Thead and Thread for Matter is not clear.

Which is the right one for the Github Lighting example?

Best regards,

 

Achim

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Remy ISSALYS
ST Employee

Hello, 

To work with Matter over Thread, you should use the X-CUBE-MATTER available on ST website. To have more details on each binary you can refer to the release notes, for Matter you should use the binary available in the X-CUBE-MATTER:

  • stm32wb5x_BLE_Thread_light_dynamic_fw.bin : Dynamic Concurrent Mode BLE Thread for Matter (Supports BLE so Stack 5.2 certified and Minimal Thread Device ready v1.3)

Best Regards