Skip to main content
satyam9896
Associate III
April 16, 2025
Question

HAL_FLASHEx_Erase() – STM32L072

Hi STM32 Community,

I'm working with the STM32L072 MCU which has 192KB of Flash. I'm implementing a bootloader + dual app OTA architecture. Here's my current memory layout:

Region Start Address End Address Description

Bootloader0x080000000x08002FFFStatic bootloader
App10x08003000-0x08002FFFCurrently running app
App2 (OTA)0x080190000x0802EFFFTarget for OTA

as per detasheet: 
Each sector is 4KB, containing 32 pages of 128 bytes each.
From App1, I'm trying to erase App2’s flash region using HAL_FLASHEx_Erase().
so oviusly in system file of app 1 the vector offset is set at 0x3000.
flashbase is defines as default 0x08000000
inkiel option for setting conf: ROM1 start -> 0x3000 and size as 0x18FFF bcz i need 88kb atleast for app1.
Here’s my erase logic:
but my while checking in debug mode the code end at error and stuck at while(1)

#define FLASH_PAGE_SIZE 128U
#define FLASH_USER_START_ADDR 0x08019000U
#define FLASH_USER_END_ADDR 0x0802EFFFU

void Flash_Erase_CodeB(void)
{
 uint32_t PageError = 0;
 FLASH_EraseInitTypeDef EraseInitStruct;

 // Unlock Flash
 HAL_FLASH_Unlock();
	 __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_PGAERR);
		__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_WRPERR );
		__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_FWWERR);
		__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_NOTZEROERR);

 // Setup erase parameters
 EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
 EraseInitStruct.PageAddress = FLASH_USER_START_ADDR/*(FLASH_USER_START_ADDR - 0x08000000U) / 128*/; // Page number
 EraseInitStruct.NbPages = (FLASH_USER_END_ADDR - FLASH_USER_START_ADDR + 1) / 128;

 if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK)
 {
 // Erase Error
 /*uint32_t*/ err = HAL_FLASH_GetError();
 // Handle error here (e.g., blink LED or reset)
 while (1);
 }

 // Lock Flash again
 HAL_FLASH_Lock();

 

This topic has been closed for replies.

4 replies

TDK
April 16, 2025

What does HAL_FLASH_GetError say is the problem? What address is reported in PageError?

"If you feel a post has answered your question, please click ""Accept as Solution""."
satyam9896
Associate III
April 17, 2025

IN ERR VAR IM GETTING VALUE 0X00000002 WHICH IS 0X2 AND IT DENOTES WRITE PROTECTION ERR BUT I HAVE CHECKED IN CUBE PROGRAMMER BEFORE FLASHING BUT THERE WAS NO ob WAS ENABLED.

err = HAL_FLASH_GetError()

 

TDK
April 17, 2025

It sounds like write protection is enabled.

Show the values of the option byte registers.

"If you feel a post has answered your question, please click ""Accept as Solution""."