cancel
Showing results for 
Search instead for 
Did you mean: 

Typo on the RM0434 Rev14

Issamos
Lead III

Hello ST Community Team. 
First of all, I want to thank you for the new AI plug-in. It is really helpful specially will looking for informations on the STM32 documents. We hope to have the same for other ST products. 

About the Typo, on the Table 1 of the RM0434, we have a reserved region between SRAM1 and SRAM2a (from 0x2000 3000 and 0x2002 FFFF) this region is included on the SRAM1 (between 0x2000 0000 and 0x2002 FFFF) so it should be mentioned if it is reserved or not g(more details needed) also the size is 180Kbytes and not 36KBytes as mentioned on the Doc.

please have a look at this.

Best Regards.

II

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Issamos 

Thank you for rising this up.

I've escalated this request internally (through ticket number: 222069) to update the RM0434 in the coming releases. (PS: Ticket number: 222069 is an internal tracking number and is not accessible or usable by customers).

 

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

1 REPLY 1
Imen.D
ST Employee

Hello @Issamos 

Thank you for rising this up.

I've escalated this request internally (through ticket number: 222069) to update the RM0434 in the coming releases. (PS: Ticket number: 222069 is an internal tracking number and is not accessible or usable by customers).

 

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen