cancel
Showing results for 
Search instead for 
Did you mean: 

Test software for RF test specified in AN5796 - STM32WL Series RF Bench

DuckTape12
Associate

Hello,

I would like to perform a LoRa Radio tests described in AN5796 - STM32WL Series RF Bench, but I do not find the needed files. So could you please share a link to firmware(STM32WL...) and software(python script and RSSMBV100 waveform).

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @DuckTape12 and welcome to the ST Community

For the Python script, you can find it on the attachment file.

For the Firmware it is the LoRaWAN_AT_Slave that you should be using. It is available on the STM32CubeWL.

For the RF instruments, we are using the R&S®FSV signal and spectrum analyzer | Rohde & Schwarz (rohde-schwarz.com) as Spectrum analyzer and the R&S®SMBV100B vector signal generator | Rohde & Schwarz (rohde-schwarz.com) as Signal generator.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @DuckTape12 and welcome to the ST Community

For the Python script, you can find it on the attachment file.

For the Firmware it is the LoRaWAN_AT_Slave that you should be using. It is available on the STM32CubeWL.

For the RF instruments, we are using the R&S®FSV signal and spectrum analyzer | Rohde & Schwarz (rohde-schwarz.com) as Spectrum analyzer and the R&S®SMBV100B vector signal generator | Rohde & Schwarz (rohde-schwarz.com) as Signal generator.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

DuckTape12
Associate

Thanks for the reply and provided files!