cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WLE5JCI6 with LoRa-E5 Development Kit.

cube_lover
Associate

Hi techs,
 I have a problem with the LoRa configuration with the LoRa-E5 Development Kit. How to do the Pin configuration for the LoRa point to point communication. I have tried multiple ways to do but the communication is not happening, and I also tried the PA4 = 0 and PA5 = 1 pins are in Tx mode. I have used the CubeMX for HAL code generation. Can anyone tell how to do? 

0 REPLIES 0