cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL5MOC LSE 32kHz accuracy

50_ohm
Associate
Hi, 
 
In the STM32WL5MOC datasheet I can find the 32MHz TXCO HSE accurancy, but not the LSE 32kHz RTC clock accuracy. Could someone look into this and provide the min/max values similar to TXCO characteristics in Table 10?
 
Best Regards,
Dave
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @50_ohm, to the community!

I am very sorry that this specification is not mentioned in the data sheet. However, I would like to point out that the frequency accuracy of the 32MHz HSE is an essential prerequisite for proper functioning in some frequency bands.

The built-in LSE crystal has a frequency tolerance of ±20ppm at 25°C and a parabolic coefficient of -0.04ppm/°C². If there are any deviations, you can use the smooth calibration function included in the built-in STM32WL55JC, together with the temperature sensor if necessary. I have also explained the smooth calibration in a more understandable way in this thread. There is also a Knowledge Base article describing the smooth calibration for the STM32U575 which uses a similar RTC.

Hope this answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @50_ohm, to the community!

I am very sorry that this specification is not mentioned in the data sheet. However, I would like to point out that the frequency accuracy of the 32MHz HSE is an essential prerequisite for proper functioning in some frequency bands.

The built-in LSE crystal has a frequency tolerance of ±20ppm at 25°C and a parabolic coefficient of -0.04ppm/°C². If there are any deviations, you can use the smooth calibration function included in the built-in STM32WL55JC, together with the temperature sensor if necessary. I have also explained the smooth calibration in a more understandable way in this thread. There is also a Knowledge Base article describing the smooth calibration for the STM32U575 which uses a similar RTC.

Hope this answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.