STM32WBA family use of stack BLE without LSE (with LSI2)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-30 1:33 AM
Hi to all!
We are developing a low-cost application, with in mind STM32WBA52KE, which use a 32 pin package.
Due to short number of pin, we would use pin 12 and 13 as GPIO, so we should not use the LSE.
Is it possible to manage the BLE stack without LSE, using LSI2? If yes, which kind of limitation we will have?
I can't find the right answer on documentation, can you help me?
Thank you very much in advance.
- Labels:
-
STM32WBA series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-30 3:24 AM - edited ‎2024-11-08 8:14 AM
Hello @Wladimiro_Gaiotti and welcome to the ST Community.
Yes, you can implement a BLE application using the STM32WBA52 without LSE. In this case, you will have to use HSE/1000 as clock source for the radio sleep timer clock. As mentioned on the release note of STM32CubeWBA package v1.4.1, LSI2 is not supported as clock source for the radio sleep timer clock. Using HSE also will limit you on Low power modes to sleep mode.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-06 5:50 AM
Hi @STTwo-32,
- Implemented near similar case, that not used LSE, results issue in BLE connection.
- As BLE requires Radio Sleep Timer Clock, for which two options available:
Option-1. HSE/1000: Implemented, tested and found that BLE advertisement works but connection not works.
Option-2. LSE: Implemented, tested and found that BLE advertisement and connection works perfectly.
Seems, LSE is mandatory for BLE operations.
- Further, in reference manual mentioned that LSI2 is available for STM32WBA54/55xx devices,
Means, not available for STM32WBA52xx devices:
- Can you please provide guidance, related to which source require for Radio-Sleep-Timer-Clock,
And how to make BLE working properly, is that further configuration requires?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-08 8:16 AM
Hello @rajdeep_01
Maybe my first answer was not clear. I've updated my answer with more details that you may check.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-09 8:39 AM
Hi @STTwo-32,
Thanks for quick reply,
But unfortunately, with HSE/1000 as source, BLE not working properly, in this case, application able to capture BLE advertisement data but not able to connect over BLE, every time connection timeout occurs, scenario is reproduceable,
only upon LSE as radio-sleep-time clock-source working properly,
I have tried multiple times with different boards, applications & mobiles,
tested with Nucleo-WBA52CG, App ST-BLE-Toolbox.
It will be really helpful in case, you will able to provide a working example where HSE/1000 configured for Nucleo-WBA52CG, you can use existing examples, such as p2p_server_ota where LSE clock used and only modify related to HSE/1000 and test.
Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-30 1:06 AM
@STTwo-32
Note that HSE/1000 as clock source for radio sleep timer clock, does not solve BLE issue,
in that case, it's able to BLE advertisement properly but not able to connect over BLE.
- Board: NUCLEO-STM32WBA52
- MCU: STM32WBA52CGUX
- SDK: 1.1.1
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-30 1:40 AM - edited ‎2024-12-30 1:49 AM
Hello @rajdeep_01
Please note that the NUCLEO-WBA52CG is an obsolete product. If you want to have a full support with all driver issues solved, please use the NUCLEO-WBA55CG.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-30 1:56 AM
@STTwo-32
Let's stick with issue that strictly related to STM32WBA52 MCU,
for which STM claims 10-Year-Production-Life support.
Hope STM will fix the issue or acknowledge issue and will update same in related errata in next release.
Also requesting to unmark accept as solution:
2024-07-30 03:24 AM - edited ‎2024-11-08 08:14 AM
Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-30 2:11 AM
Hello @rajdeep_01
The STM32WBA52 MCUs are still supported. It is just the Nucleo evaluation board that has been marked as obsolete. we will always keep updating our errata documents if there is any limitation on our product. But for now, we dont have any one except those who are already on our errata doc.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 3:07 AM - edited ‎2025-03-27 3:20 AM
Hi @rajdeep_01 , Hi @Wladimiro_Gaiotti ,
Let me update this old topic with some news :
I confirm there is two valid options to run BLE over STM32WBA52 without LSE. Both solutions are validated for BLE.
- Option #1 : Running using HSE_DIV100
I do confirm that it is possible to use HSE_DIV1000 for BLE.
PeriphClkInit.RadioSlpTimClockSelection = RCC_RADIOSTCLKSOURCE_HSE_DIV1000;
Of course, using HSE_DIV1000, it is no more possible to mange low_power_mode as HSE must remains always active.
Low power mode must so be disabled :
#define CFG_LPM_LEVEL (0)
To ease testing of HSE_DIV1000 over CubeFW code example, you may use attached .pdf doc - I tested it on STM32CubeFW code example running over Nucleo-WBA55 board (tested using BLE_P2P_Server and BLE_HeartRate) code examples.
- Option #2 :Running using LSI2
Since last CubeFW delivery v1.6, LSI2 usage is now possible.
More details here : https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WBA_without_LSE_crystal
Regards,
Sebastien.