STM32WB5MMGHx custom app couldn't go back to OTA Loader App
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-08 9:40 PM
I am following this video link showing step by step to create OTA app.
https://www.youtube.com/watch?v=mRzZOa3jmuM.
I am successfully to create the custom application, download the OTA loader app at 0x08000000, and the custom's app at 0x08007000. The problem I am facing is whenever I sent some data to OTA Reboot characteristic, the custom app is just reset, then go back to the custom app. It didn't enter the OTA loader app. Am I missing something like the erase current app function? I also notice in my custom app, once the ST BLE tool box or ST BLE Sensor app connects to my device, it didn't show the OTA reboot option like when I tried the BLE_p2pServer_ota.
Solved! Go to Solution.
- Labels:
-
STM32WB series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 2:38 AM
Thank you Axel.
I found the bug. My copied and pasted code mistake so I used the Notification characteristic for the Reboot Mode characteristic which is the problem I will never got the command sent in from ST ToolBox BLE app.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-09 2:10 AM - edited ‎2023-11-20 6:00 AM
So I found this info,
When my device is up, it has the option "OTA Reboot Request" when I use ST Ble Toolbox,
I write Hex "000702" but nothing is happening
My code has
case CUSTOM_STM_BOOT_REQUEST_EVT:
*(uint32_t*)(SRAM1_BASE) = *(uint32_t*)pNotification->DataTransfered.pPayload;
NVIC_SystemReset();
break;
Do I understand the logic is OTA loader will use the information from SRAM1_BASE (which is define at 0x20000000UL, to erase my 2 sector starting at 0x08007000?
#define SRAM_BASE (0x20000000UL)/*!< SRAM(up to 256 KB) base address */
#define SRAM1_BASE SRAM_BASE /*!< SRAM1(up to 192 KB) base address */
If I used the programmer, and manually erased 2 sectors starting from 0x08007000, after the power cycle, my device always comes up with STM_OTA which is the OTA loader application was loaded at 0x08000000.
Please suggest where should I need to double check or my errors.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 2:33 AM - edited ‎2023-11-20 6:00 AM
Hello @Jtron.1​ ,
Please not that I am not an expert of BLE or OTA, but from my own experience I could give you some advises.
First of all, may I have for information about your configuration?
What MCU are you using, running on an EVAL board ? What binary OTA application do you flash ? It is the last release ?
For the following I am assuming that your are running an custom BLE application.
Here is the general idea of procedure for OTA application:
- {Ensure your BLE stack is update and running}
- Flash OTA application at @0x08000000
- Add OTA reboot characteristic to one of your BLE service
- Managed the OTA reboot characteristic
In custom_app.c:
...
case CUSTOM_STM_OTA_REBOOT_REQUEST_WRITE_EVT:
/* USER CODE BEGIN CUSTOM_STM_OTA_REBOOT_REQUEST_WRITE_EVT */
APP_DBG_MSG("\r\n\r** OTA Reboot event!\n");
/* Write reboot reason at 0x20000000 (SRAM1):
* Boot Mode: 0x00-> User Application (0x08007000), 0x01-> OTA application (0x08000000)
* Sector index: 0x07 (7 sectors is the first to be program)
* Number of sector to be erase (4K granulation): Filesize/4K + 1
* Total: 3bytes (octets).
* */
*(uint32_t *)SRAM1_BASE = *(uint32_t*)pNotification->DataTransfered.pPayload;
NVIC_SystemReset();
while(1);
/* USER CODE END CUSTOM_STM_OTA_REBOOT_REQUEST_WRITE_EVT */
break;
...
- Managed the vector table relocation (or not?)
In /Core/Src/system_stm32wbxx.c
...
#define USER_VECT_TAB_ADDRESS
#if defined(USER_VECT_TAB_ADDRESS)
/*!< Uncomment this line for user vector table remap in Sram else user remap
will be done in Flash. */
/* #define VECT_TAB_SRAM */
#if defined(VECT_TAB_SRAM)
#define VECT_TAB_BASE_ADDRESS SRAM1_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00007000U /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#endif /* VECT_TAB_SRAM */
#endif /* USER_VECT_TAB_ADDRESS */
- Modify linkerscript (STM32WB5xx_FLASH.ld file) to add the magic keyword section
...
.ota_region 0x08007140:
{
KEEP(*(TAG_OTA_START))
. = ALIGN(4);
} >FLASH
...
.ota_region_end :
{
. = ALIGN(4);
KEEP(*(TAG_OTA_END))
. = ALIGN(4);
} >FLASH
...
- In app_ble.c
/**
* These are the two tags used to manage a power failure during OTA
* The MagicKeywordAdress shall be mapped @0x140 from start of the binary image
* The MagicKeywordvalue is checked in the ble_ota application
*/
PLACE_IN_SECTION("TAG_OTA_END") const uint32_t MagicKeywordValue = 0x94448A29 ;
PLACE_IN_SECTION("TAG_OTA_START") const uint32_t MagicKeywordAddress = (uint32_t)&MagicKeywordValue;
- Ensure your MagicKeyword is correctly written (using STM32CubeProgrammer for exemple)
You may see the OTA procedure describe in this figure
AN5247 may be usefull for you.
BeST Regards,
Axel L.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 2:38 AM
Thank you Axel.
I found the bug. My copied and pasted code mistake so I used the Notification characteristic for the Reboot Mode characteristic which is the problem I will never got the command sent in from ST ToolBox BLE app.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 2:42 AM
Glad that you resolve your problem.
May you flag this question as answer, this can help other people.
BeST Regards,
Axel L.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 2:55 AM
Axel,
May I ask you couple questions regarding the ST BLE toolbox or Sensor app?
- When I tested either with HeartRate_ota or P2P_Server_ota, the 2 app nicely provide more button and calculate the parameters in the background to send to the application to back to STM_OTA.
Is this proprietary from ST? Or there are any App Note that share the information.
Is the feature depending on the specific UUID it receives?
In my custom template app, I have 1 service: 2 characters: write and notification. Doesn't matter what UUID I assigned but when I used FULL 128 bits, my write characteristic always show the same UUID as the notification characteristic.
If I changed them back to reduce, I then see 2 different UUID (2 bytes) for each of characteristics.
Do you know why?
Or do you know any App Note to elaborate the UUIDs?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 3:24 AM
Sure, if I can help,
From what I experience:
- ST BLE Toolbox/sensor are develop by ST. I thinks that the app managed alone the command because the UUID is standard for OTA procedure so the app recognize it. I don't know well about theses two apps.
- When creating services you have two options:
- Use standards UUID publied and reference by the SIG, so you can use the reduce for on 16-bits (for exemple Heart rate service is 0x180D). I attach for you a document that describe the standards UUID.
- Generate random UUID for you own custom services/caracteristics. Please not that is it mandatory to not use a standard service UUID for your custom services UUID. You can find online custom UUID generator.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 3:30 AM
Thank you Axel,
That is my problem. I generate 128 bit of UUID for my own, I used it for Service, Write, and Notification characteristics but ST BLE tool box pickup and use the same UUID for Write and Notification. I don't understand this.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 3:34 AM
Please pay attention that you need to generate a custom UUID for you #Service1 then generate customs UUIDs for you characteristic #CharA, and #CharB.
As a result of the previous example, you will have a custom service #Service1 that contain two characteristics: #CharA and #CharB.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-05-11 3:40 AM
Thank you so much for your help. I might not clear in my previously post.
I generated for example EEAABB01-0000-0000.., I used for Service 1 then I just change EEAABB02- 0000-0000.., and EEAABB02-0000-0000.., for CharA and CharB respectively.
Still the ST BLE toolbox app pick only EEAABB02-0000-0000.., to show on the app for both Char.