2024-05-01 11:26 PM
I have multiple questions:
1. Is there a limit on the firmware size in STM32WB series? If yes, what is the limit?
2. Is there a limit on the firmware size of the OTA application in STM32WB series? If yes, what is the limit?
3. I want to perform OTA at a different address, not 0x08007000. Is it possible?
2024-06-02 10:26 AM
Hello @Lalit1
I suggest you to take a look at the recommandations of the AN5247 and the following MOOC. They should be the best guides for your questions.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.