2022-05-15 07:00 PM
Note: I can use stlink to download programs to other boards.But p_nulceo_wb55 doesn't work well. I use an external stlink instead of the on-board stlink, the errors are same.
I was learning Bluetooth, It would have worked well. After a while, an error has occurred.
Is it because I have downloaded some program?
The errors are as follows(use stm32cubeprogrammer ):
the erros in stm32cubeide:
2022-06-23 01:31 AM
Hello,@Sara BEN HADJ YAHYA (ST Employee)
I have posted a lot about these problems, and these methods are not working.I only remember downloading the BLE example at the time, and then the next day there was this failure.
Thanks,
Lep