cancel
Showing results for 
Search instead for 
Did you mean: 

I want to reset and reinitialize only CPU2 (M0 +) of STM32WB

MNitt.1
Associate II

I want to reset and reinitialize only CPU2 (M0 +) of STM32WB

I used to ask a question in "Data reception stops at Mac_802_15_4_FFD in the sample code."

Even now, this matter has not been resolved.

At the end, it was said that RFD was used, but since I want to communicate with FFD, I have not confirmed it with RFD.

I would like to resolve this phenomenon, but if I can confirm this phenomenon with F/W, I would like to reset and reinitialize only CPU2.

Is such a thing possible? How can I do it?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MNitt.1
Associate II

I forgot to write one point, but the communication packet received by "Data reception stops at Mac_802_15_4_FFD in the sample code." Is sent by broadcast.