cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 - ACI_HAL_TONE_START command rf channel resolution

serhat
Associate II

Hi everyone,

I use STM32WB55 with the BLE stack 13.0 (full version) and want to test the RF. In the an5270 document, I noticed the ACI_HAL_TONE_START command and it is allowed to change the rf channel from 2.402 to 2.480 GHz with 2 MHz resolution. However, I want to change the channel to a 1 MHz resolution. For example, I want to set the channel to 2.403 GHz. Is it possible to do? If yes, how?

Thank you.

Have a nice day.

Serhat.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Remy ISSALYS
ST Employee

Hello,

The BLE system uses 40 RF channels, with 2 MHz spacing, so it's not possible to have a 1 MHz resolution.

Best Regards

View solution in original post

1 REPLY 1
Remy ISSALYS
ST Employee

Hello,

The BLE system uses 40 RF channels, with 2 MHz spacing, so it's not possible to have a 1 MHz resolution.

Best Regards