2025-03-03 2:17 AM - last edited on 2025-03-03 5:47 AM by STTwo-32
I've been using B-WB1M-WPAN board with a modified example of motion service from BLE_HR_p2p_Sensor. but with IMU readings with a steval-mki217v1 shield connected with SPI.
So far I have been able to read IMU data and send it through a BLE notifiacation service. but when I try to setup a MotionFx server it mulfunctions.
here are some combinations I've tried. with this line of code MotionFX_initialize((MFXState_t *)mfxstate);
1. when initialize after MX_APPE_Init(); in main.c the device will enter a hardfault error in couple of loops. same goes when put on app context init.
2. when initialize before MX_APPE_Init(); it does not process the registered UTIL_SEQ_RegTask. But the davice works fine.
I already have the CRC checked from CubeMX generation.