2024-11-05 1:05 AM
Hello.
Im having issues generating an event when pressing read on my smartphone, on my CHAR_PROP_READ characteristic in my BLE service.
I enabled the "GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP", which should notify when a read request of any type is received for this attribute. When i build the project and debug in the service_EventHandler for this service, it shows that the eventhandler is never entered when clicking read. I do receive the value that is initialized, so communication is working.
When i test the "GATT_NOTIFY_WRITE_REQ_AND_WAIT_FOR_APPL_RESP" for the write equivalent event, this works just fine, so its just the read event that is not generated.
Any idea why im not getting an event when reading?
2024-11-20 10:20 AM
Hello @s215477
I've escalated your request internally for more details (under internal ticket number 196695). In the meantime, you may want to take a look at this post (an STM32WB55 case that may help you but I'm not sure).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-03 8:13 AM
Hello @s215477
The GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP is used in network coprocessor context: when a read request arrives, the ACI_GATT_SRV_AUTHORIZE_NWK is notified in order to authorize the read with the aci_gatt_srv_authorize_resp_nwk() API.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.