cancel
Showing results for 
Search instead for 
Did you mean: 

STM32cubemonitorRF - 'Get RSSI' disabled

ljm
Associate III

Hello

i'm using STM32WB05KZ (nucleo board) : Nucleo-WB05KZ with STM32CubemonitorRF

Please why here i can't select  "Get RSSI" , it's locked ?

ljm_0-1741690654359.png

and other question how can i modifie the outpout power (TX) of the antenna ( dBm) ? 

thank you 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @ljm 

The Get RSSI option is locked due to the Firmware implementation on the STM32WB0, the ACI_HAL_READ_RSSI command is not supported.

For the second question, if you are testing on a transmitter, you can set the PA Level you want here:

STTwo32_0-1741774312154.png

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
STTwo-32
ST Employee

Hello @ljm 

The Get RSSI option is locked due to the Firmware implementation on the STM32WB0, the ACI_HAL_READ_RSSI command is not supported.

For the second question, if you are testing on a transmitter, you can set the PA Level you want here:

STTwo32_0-1741774312154.png

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

hello

thanks for replying.

for "Get RSSI" means there is no solution to get the RSSI value ?

i do the some in mode transmission, i get the number of packets but there is no value for the rssi : 

ljm_0-1741775471767.png

thanks

For the STM32WB0, you can't get the RSSI using the STM32CubeMonitorRF. 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello 

thanks for replyong

For the Nucleo STM32WB05KZ board, the transmission power is normally 0 dBm by default (it can go up to 8 dBm).

Is it possible to modify the transmission power according to my needs, for example to 3 or 4 dBm, using STM32CubeProgrammer or another software?

thanks 

As I said before, for each new question, is always better to create a new post. So, please create a new post (after closing the questions that you have already posted and that get answered).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Super User

New Post here: https://community.st.com/t5/stm32-mcus-wireless/stm32wb05kz-power-antenna-modification/td-p/782104

 

@ljm Don't forget to mark a solution in this thread!

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.