cancel
Showing results for 
Search instead for 
Did you mean: 

SHCI_C2_BLE_Init Fails

TWood.4
Associate III

I'm trying to start up CPU2 on an STM32WB55. I've looked at various examples and I seem to be doing all the right things.

SHCI_C2_BLE_Init returns 0xFF in payload[0] which corresponds to SHCI_FUS_CMD_NOT_SUPPORTED

I have FUS V1.2.0.0 installed and the Full BLE stack V1.15.03 installed, which I can start and run from the STM32CubeProgrammer.

Advice on how to debug this would be welcome.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Remy ISSALYS
ST Employee

Hello,

If you try with an example available in STM32CubeWB package, is it working?

Best Regards