2024-02-08 03:57 AM
Hi,
I just want to know whether STM32WB5MMG module supports LE Audio since it has Bluetooth LE 5.4. If it supports can anyone help how to do it.
Thanks and Regards,
LR.2
Solved! Go to Solution.
2024-02-08 06:49 AM
Hi Lr.2,
As mentioned in STTwo-32, the STM32WB5MMG module supports an audio solution based on the Opus codec.
If you are interested in Auracast/LE Audio, you should look into the STM32WBA.
There are already two applications that you can find here.
A new board, the STM32WBA Audio Discovery Kit, will be available around mid-March 2024.
And new examples will be published at the same time, such as the BLE_Audio_TMAP_Unicast_Server.
BR, Joé
2024-02-08 06:39 AM - edited 2024-02-08 07:00 AM
Hello @LR.2
The STM32WB5MMG module support the audio solution based on the Opus codec. For the LE Audio, you can find an answer here. You can find a support for the LE AUDIO on the STM32WBA.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-08 06:49 AM
Hi Lr.2,
As mentioned in STTwo-32, the STM32WB5MMG module supports an audio solution based on the Opus codec.
If you are interested in Auracast/LE Audio, you should look into the STM32WBA.
There are already two applications that you can find here.
A new board, the STM32WBA Audio Discovery Kit, will be available around mid-March 2024.
And new examples will be published at the same time, such as the BLE_Audio_TMAP_Unicast_Server.
BR, Joé
2024-02-11 09:41 PM - edited 2024-02-11 10:33 PM
Hi Joe,
Thanks for the reply. I'm looking forward to try STM32WBA Audio Discovery Kit and also, I want to know is there any plan to release module for STM32WBA?
Regards,
LR.2