cancel
Showing results for 
Search instead for 
Did you mean: 

Reading the Seeed Studio LoRa-E5 docs they talk about SX1262 "It is powered by ARM Cortex-M4 core and Semtech SX126X LoRa chip" yet they have a STM32WLE5JC? Isn't the STM32WLE5JC a M4+Radio? The NUCLEO-WL55JC2 doesn't have a SX1262 yet it does (G)FSK..

KevinA
Senior
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

It's not an SX1262 chip, but IP on the same die which is materially very similar, with an internal SPI connection.

Some variants have LoRa functionality disabled, to reduce costs related to licencing.

https://www.st.com/en/microcontrollers-microprocessors/stm32wl-series.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KevinA
Senior

After doing a lot of reading I finally found LoRa, which defines FHSS and then I came across a ST statement that only certain STM32WLx5xx devices do LoRa, the NUCLEO-WL55JC2 does and I added a P-NUCLEO-LRWAN2 for a gateway. Should keep me busy a day or two.

I'm glad to see ST adding that IP, now if they could talk to ambiq about 4ua/Mhz running ...