2023-12-08 2:50 AM
In the STM32CubeWB source code collection, I found the BLE_Peripheral_Lite project. This project however is only available for the P-NUCLEO-WB55, but I am working with the NUCLEO-WB15 board.
According the Release notes this should be easy:
<quote>
The provided examples can be tailored to run on any compatible hardware; user simply need to update the BSP drivers for his board, if it has the same hardware functions (LED, LCD display, pushbuttons...etc.). The BSP is based on a modular architecture that allows it to be ported easily to any hardware by just implementing the low level routines.
</quote>
My question is: How do I update the BSP drivers for my board?
BR, Ben
Solved! Go to Solution.
2023-12-10 10:35 PM
Hello @_Ben and welcome to the ST Community :smiling_face_with_smiling_eyes:.
For a successful migration, you have to take care of some differences in hardware, peripheral availability, firmware, security, and tools. You can use the AN5805 for a smooth migration.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-10 10:35 PM
Hello @_Ben and welcome to the ST Community :smiling_face_with_smiling_eyes:.
For a successful migration, you have to take care of some differences in hardware, peripheral availability, firmware, security, and tools. You can use the AN5805 for a smooth migration.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-11 1:12 AM - edited 2023-12-11 1:13 AM
For clarity: It turns out that the phrase "user simply need to update the BSP drivers for his board" from the release notes is a bit optimistic in the sense that it is not just replace file X with file Y, but requires a few hours of checking and configuring stuff, provided you know what you are doing.